This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C EEPROM



我在进行写操作时,程序一直处在I2caRegs.I2CMDR.bit.STP=1;状态,导致我无法进行写操作,

I2CA_WriteData(struct I2CMSG *msg) 

  int16 i;

while (I2caRegs.I2CMDR.bit.STP == 1)
{

return i_ERROR;
}
}

  • 硬件设计有问题吗    IIC上有没有上拉电阻等  

    附件是详细指导说明   看看

    TI__TMS320C2000__I2C模块参考指南.pdf
  • 我再单步调试例子程序时,进行写操作:当运行完I2caRegs.I2CMDR.all = 0x6E20;-----当运行完这一步后,我通过watch window,看,为何I2caRegs.I2CMDR.all = 0x4220?,请看源程序:

    Uint16 I2CA_WriteData(struct I2CMSG *msg)
    {
       Uint16 i;

       // Wait until the STP bit is cleared from any previous master communication.
       // Clearing of this bit by the module is delayed until after the SCD bit is
       // set. If this bit is not checked prior to initiating a new message, the
       // I2C could get confused.
       if (I2caRegs.I2CMDR.bit.STP == 1)
       {
          return I2C_STP_NOT_READY_ERROR;
       }

       // Setup slave address
       I2caRegs.I2CSAR = msg->SlaveAddress;

       // Check if bus busy
       if (I2caRegs.I2CSTR.bit.BB == 1)
       {
          return I2C_BUS_BUSY_ERROR;
       }

       // Setup number of bytes to send
       // MsgBuffer + Address
       I2caRegs.I2CCNT = msg->NumOfBytes+2;

       // Setup data to send
       I2caRegs.I2CDXR = msg->MemoryHighAddr;
       I2caRegs.I2CDXR = msg->MemoryLowAddr;
    // for (i=0; i<msg->NumOfBytes-2; i++)
       for (i=0; i<msg->NumOfBytes; i++)

       {
          I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
       }

       // Send start as master transmitter
       I2caRegs.I2CMDR.all = 0x6E20;-----当运行完这一步后,我通过watch window,看,为何I2caRegs.I2CMDR.all = 0x4220?

       return I2C_SUCCESS;
    }

  • 探索者 说:

    我再单步调试例子程序时,进行写操作:当运行完I2caRegs.I2CMDR.all = 0x6E20;-----当运行完这一步后,我通过watch window,看,为何I2caRegs.I2CMDR.all = 0x4220?,请看源程序:

    Uint16 I2CA_WriteData(struct I2CMSG *msg)
    {
       Uint16 i;

       // Wait until the STP bit is cleared from any previous master communication.
       // Clearing of this bit by the module is delayed until after the SCD bit is
       // set. If this bit is not checked prior to initiating a new message, the
       // I2C could get confused.
       if (I2caRegs.I2CMDR.bit.STP == 1)
       {
          return I2C_STP_NOT_READY_ERROR;
       }

       // Setup slave address
       I2caRegs.I2CSAR = msg->SlaveAddress;

       // Check if bus busy
       if (I2caRegs.I2CSTR.bit.BB == 1)
       {
          return I2C_BUS_BUSY_ERROR;
       }

       // Setup number of bytes to send
       // MsgBuffer + Address
       I2caRegs.I2CCNT = msg->NumOfBytes+2;

       // Setup data to send
       I2caRegs.I2CDXR = msg->MemoryHighAddr;
       I2caRegs.I2CDXR = msg->MemoryLowAddr;
    // for (i=0; i<msg->NumOfBytes-2; i++)
       for (i=0; i<msg->NumOfBytes; i++)

       {
          I2caRegs.I2CDXR = *(msg->MsgBuffer+i);
       }

       // Send start as master transmitter
       I2caRegs.I2CMDR.all = 0x6E20;-----当运行完这一步后,我通过watch window,看,为何I2caRegs.I2CMDR.all = 0x4220?

       return I2C_SUCCESS;
    }

    bit13,11置位后自动清零,bit12位为保留位,读取始终为0

  • 硬件加了上拉电阻10k,同样的程序在不同的2808板子上可以,但是在28035上就会I2caRegs.I2CMDR.bit.STP =1,是否等于1软件是无法配置的吧?

    Uint16 I2CA_WriteData(struct I2CMSG *msg)
    {
       Uint16 i;

       if (I2caRegs.I2CMDR.bit.STP == 1)
       {
          return I2C_STP_NOT_READY_ERROR;
       }

       // Setup slave address

    。。。。。。。。。。。。。。。。。。。

    }

  • 恩,谢谢,我还发现在ccs中单步调试时 读取数据时 I2caRegs.I2CSTR.bit.ARDY=0;而全速运行模式时 I2caRegs.I2CSTR.bit.ARDY=1,为何有这样的区别啊