This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI FIFO



我想让SCI 通过FIFO在不中断的情况下,一次存入8个数据。不知道下面的程序存在什么问题?谢谢!

#include "DSP2833x_Device.h"   
#include "DSP2833x_Examples.h"  


void scia_fifo_init(void);

Uint16 rdataA[8];

 

void main(void)
{
  Uint16 i;
   InitSysCtrl();

   InitSciaGpio();

   DINT;

   InitPieCtrl();

   IER = 0x0000;
   IFR = 0x0000;

   InitPieVectTable();
scia_fifo_init();

for(i=0;i<8;i++)
{
rdataA[i]=0;
}


while(1)

 {
 //  while(SciaRegs.SCIRXST.bit.RXRDY !=1) { }
 //  a= SciaRegs.SCIRXBUF.all;
while (ScicRegs.SCIFFTX.bit.TXFFST != 8) {}
for(i=0;i<8;i++)
{

rdataA[i]=SciaRegs.SCIRXBUF.all;

}

 }

}

void scia_fifo_init()
{

  SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback
 
 SciaRegs.SCICTL1.all =0x0003;
    SciaRegs.SCICTL2.bit.TXINTENA = 1;
 SciaRegs.SCICTL2.bit.RXBKINTENA =1;
 SciaRegs.SCIHBAUD    =0x0001;  // 9600 baud @LSPCLK = 37.5MHz.
 SciaRegs.SCILBAUD    =0x00E7;
    SciaRegs.SCICCR.bit.LOOPBKENA=1;
    SciaRegs.SCIFFTX.all=0xC028;
    SciaRegs.SCIFFRX.all=0x0028;
    SciaRegs.SCIFFCT.all=0x0;

 SciaRegs.SCICTL1.all =0x0023;  // Relinquish SCI from Reset
    SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
    SciaRegs.SCIFFRX.bit.RXFIFORESET=1;

}