This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS3.3下载28335程序

1.自己做的一块28335的PCB,使用XDS510PLUS下载SCI程序,程序下载好以后在在线调试的run和animate状态程序在运行,可以与串口调试助手互发数据。

可是如果在run状态下halted之后断开连接程序不运行,reset无效;

在animate状态下disconnect可以运行,但是只要reset程序又不运行了,请问是什么原因?谢谢了 (说明:程序是合众达实验箱配套的。)

 

 2.为什么程序正常运行起来摸上去芯片挺烫的,比起我以前用的AVR或者STM32单片机热很多,但应该也没坏。功耗这么大么?用的稳压源,整版的功率也就不到1W?

谢谢!