This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问大家28335需要使用IQMath么?



大家好,之前在使用2812,由于定点处理器,所以使用了IQmath。

现在改成28335进行编程,需要使用大量正弦/余弦,不知道还需不需要使用IQmath?

另,我在另一个帖子中对28335浮点除法需要时间进行了提问,因为IQmath除法的时间可以查到,约63个周期,而不知道28335浮点运算需要多少?

谢谢大家啦。

  • 有浮点单元的 MCU, 我认为 IQmath 不是必须的了,但还可以用,如果是以前定点代码移植过来的代码,那还需要这个库。

    至于速度,正弦/余弦计算是通过傅立叶展开后计算的,循环次数不确定,不同的数值会有不完全相同的时间