This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在调试F28M35时候,M3的程序能够正常下载到flash上,而C28不能下载,ccs 6提示的错误信息为:
C28xx_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_0: File Loader: Verification failed: Values at address 0x000000000013E000 do not match Please verify target memory and memory map.
C28xx_0: GEL: File: C:\Users\MQinDong\Documents\TIccs\Projects\MMC\MMC_v2\MMC_C28_v2\FLASH\MMC_C28_v2.out: a data verification error occurred, file load failed.
我用的cmd文件是controlSUITE提供的最新版本(v206):F28M35x_headers/cmd/F28M35x_Headers_nonBIOS.cmd和F28M35x_common\cmd\F28M35H52C1_c28.cmd.
其中,F28M35H52C1_c28.cmd如下。
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
FLASHN : origin = 0x100000, length = 0x002000 /* on-chip FLASH */
FLASHM : origin = 0x102000, length = 0x002000 /* on-chip FLASH */
FLASHL : origin = 0x104000, length = 0x002000 /* on-chip FLASH */
FLASHK : origin = 0x106000, length = 0x002000 /* on-chip FLASH */
FLASHJ : origin = 0x108000, length = 0x008000 /* on-chip FLASH */
FLASHI : origin = 0x110000, length = 0x008000 /* on-chip FLASH */
FLASHH : origin = 0x118000, length = 0x008000 /* on-chip FLASH */
FLASHG : origin = 0x120000, length = 0x008000 /* on-chip FLASH */
FLASHF : origin = 0x128000, length = 0x008000 /* on-chip FLASH */
FLASHE : origin = 0x130000, length = 0x008000 /* on-chip FLASH */
FLASHD : origin = 0x138000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x13A000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x13E000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x13FF80, length = 0x000070 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x13FFF0, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
FLASH_EXE_ONLY_P0 : origin = 0x13FFF2, length = 0x000002 /* Part of FLASHA. Flash execute only locations in FLASHA */
ECSL_PWL_P0 : origin = 0x13FFF4, length = 0x000004 /* Part of FLASHA. ECSL password locations in FLASHA */
CSM_PWL_P0 : origin = 0x13FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
FPUTABLES : origin = 0x3FD258, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3FD8F8, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FE448, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FE4D4, length = 0x0000AA /* IQ Math Tables in Boot ROM */
BOOTROM : origin = 0x3FEDA8, length = 0x001200 /* Boot ROM */
PIEMISHNDLR : origin = 0x3FFFBE, length = 0x000002 /* part of boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML2 : origin = 0x00A000, length = 0x001000 /* on-chip RAM block L2 */
RAML3 : origin = 0x00B000, length = 0x001000 /* on-chip RAM block L3 */
RAMS0 : origin = 0x00C000, length = 0x001000 /* on-chip Shared RAM block S0 */
RAMS1 : origin = 0x00D000, length = 0x001000 /* on-chip Shared RAM block S1 */
RAMS2 : origin = 0x00E000, length = 0x001000 /* on-chip Shared RAM block S2 */
RAMS3 : origin = 0x00F000, length = 0x001000 /* on-chip Shared RAM block S3 */
RAMS4 : origin = 0x010000, length = 0x001000 /* on-chip Shared RAM block S4 */
RAMS5 : origin = 0x011000, length = 0x001000 /* on-chip Shared RAM block S5 */
RAMS6 : origin = 0x012000, length = 0x001000 /* on-chip Shared RAM block S6 */
RAMS7 : origin = 0x013000, length = 0x001000 /* on-chip Shared RAM block S7 */
CTOMRAM : origin = 0x03F800, length = 0x000380 /* C28 to M3 Message RAM */
MTOCRAM : origin = 0x03FC00, length = 0x000380 /* M3 to C28 Message RAM */
FLASHB : origin = 0x13C000, length = 0x002000 /* on-chip FLASH */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0
flashexeonly : > FLASH_EXE_ONLY_P0 PAGE = 0
ecslpasswds : > ECSL_PWL_P0 PAGE = 0
csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CTOMRAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > MTOCRAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > RAML2 PAGE = 1
.esysmem : > RAML2 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
DMARAML2 : > RAML2, PAGE = 1
DMARAML3 : > RAML3, PAGE = 1
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
我之后又将上述F28M35H52C1_c28.cmd替换为28M35H52C1_RAM_lnk_c28,就可以下载到RAM调试了,有谁遇到相同问题?我估计是cmd文件的问题,但不知道哪儿出错。
没有超出FLASHA的大小,因为map文件显示 FLASHA unused memory还有空间。我也尝试将代码放到更大的FLASH段,仍然出现相同问题。
MA DONG 说:没有超出FLASHA的大小,因为map文件显示 FLASHA unused memory还有空间。我也尝试将代码放到更大的FLASH段,仍然出���相同问题。
试试其他的flash版小程序,看看是否问题重现?
我也试过了,仍然出现相同的问题。
我测试的最小例程是controlSUITE里面的..\ti\controlSUITE\device_support\f28m35x\v206\F28M35x_examples_Dual\blinky目录下的例程。我也测试了controlSUITE以前版本的同名例程,v203~v206都测试了,都是相同问题。
有人说是仿真器或者芯片的原因,不知道是不是有这样的可能。如果是仿真器的原因,但是M3的代码是可以用我用的仿真器烧写到 m3 flash运行的,并且C28 core也可以在RAM里面运行,且在CCS 调试界面相关的调试操作也很正常,比如断点、停止、运行等操作,所以我觉得我的仿真器是正常的。同理,我觉得芯片出问题的可能性也较小。我现在也没办法,暂时只能让代码在RAM运行。
MA DONG 说:我也试过了,仍然出现相同的问题。
我测试的最小例程是controlSUITE里面的..\ti\controlSUITE\device_support\f28m35x\v206\F28M35x_examples_Dual\blinky目录下的例程。我也测试了controlSUITE以前版本的同名例程,v203~v206都测试了,都是相同问题。
有人说是仿真器或者芯片的原因,不知道是不是有这样的可能。如果是仿真器的原因,但是M3的代码是可以用我用的仿真器烧写到 m3 flash运行的,并且C28 core也可以在RAM里面运行,且在CCS 调试界面相关的调试操作也很正常,比如断点、停止、运行等操作,所以我觉得我的仿真器是正常的。同理,我觉得芯片出问题的可能性也较小。我现在也没办法,暂时只能让代码在RAM运行。
这样的话问题就在硬件方面了,考虑你的仿真器可以下载到ram以及其他的板子,应该是板子的问题,建议你更换其他相同的板子,或者更换一块新的芯片。另外也可以尝试一下芯片的焊接方面,看看有没什么问题。
您好,我现在刚入手DSP,遇到了与您一模一样的问题。您说是C28 FLASH损坏了?什么意思?我用另一个全新的DSP板子再试的时候还是这个问题,您知道怎么解决吗?真诚期待您的回复,谢谢。
你如果能烧写C28 Ram,M3 ram,M3 flash 而唯独不能烧写C28flash,就多半是硬件的原因,当然你需要认真检查C28 工程所用的cmd文件,确保无误,注意,经过的测试,TI controlSUITE里面的关于F28M3系列MCU的cmd是不能保证完全正确的。另外一个方法是升级或降级你的CCS版本,说不定有意外收获。
你好啊 麻烦问一下 你还有CCS6.1.1的安装包吗?或者在哪里可以下载到?我也碰到了同样的问题。期待回复,非常感谢(Verification failed: Values at address 0x000000000013E5D4 do not match Please verify target memory and memory map.)QQ:980539975