你好,在《Running an Application from Internal Flash Memory on the TMS320F28xxx DSP》中提到:
the on-chip flash memory on these devices provides effective code execution performance that is slightly less: roughly 85 – 90 MIPS on 100 MHz devices,
请问是否有针对F280X系列的同类手册,2808的程序在flash中执行速度与RAM中相差多少?
如果我想对两种介质下的程序运行周期进行测量,有没有什么比较精准的方法?