This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI,你好
现在项目中需要使用EPWM1A、2A、3A、4A、5A、6A做为正常调制输出,EPWM1B、2B、3B、4B、5B、6B做为ECAP模块的捕捉功能使用,请问这样的用法是否可以?如果的可以,需要重点关注哪几个寄存器?
补充:我现在单独测试这两块程序是好的,但是同时使用的时候就不行,PWM没输出了。
Hank Zhao 说:ePWM和eCAP的一些管脚是复用的,不能同时使用。不过eCAP还有一些管脚没有与ePWM复用,比如GPIO24~GPIO27以及GPIO48,GPIO49,可以使用这些引脚作为eCAP的管脚。
Hank,你好!
一直以为28335的引脚复用是具体到单个引脚的,这么说,在eCAP和epwm复用的这些引脚,功能选择是整体性的,不能某些引脚作为epwm,另外一些引脚作为eCAP?有没有关于这方面介绍的资料,还想知道有没有其他的复用也这样,因为从数据手册上面好像并不能看到这个信息。谢谢。