This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: 例程 USB_ex5_host_mouse

Part Number: TMS320F28379D


我将例程 USB_ex5_host_mouse通过RAM烧录到TMS320F28379D中,将USB_ex2_dev_mouse通过RAM烧录到另一28379D中,将其GPIO42与GPIO43分别进行连接,运行程序,发现设备端(TMS320F28379D)一直发送PID DATA0包,主机端(TMS320F28379D)超时无应答。我该如何进行调整,两个28379D可以正常通过USB进行通讯?例程USB_ex5_host_mouse是否可以识别到TMS320F28379D设备?

  • 您好,

          TMS320F28379D设备是您自己的板子吗?

          建议先用电脑和其他USB鼠标分别测试下载了USB_ex2_dev_mouse和USB_ex5_host_mouse的TMS320F28379D硬件。     

          可通过串口查看调试信息。

          

  • TMS320F28379D设备是我自己的核心板。

    看了您的回复,您的意思是说TMS320F28379D硬件如果运行的是USB_ex2_dev_mouse例程,可以与电脑进行连接通讯。如果运行的是USB_ex5_host_mouse例程,需要连接其他的USB鼠标,而不能与运行USB_ex2_dev_mouse例程的TMS320F28379D硬件进行通讯是吗?

  • USB_ex2_dev_mouse例程就是USB鼠标,分开测试,是让您先排查软硬件问题。