This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CodeStartBranch.asm



请问CodeStartBranch.asm,能看做是bootloader 的一部分吗?

  • DSP281X的CodeStartBranch.asm

    是Boot的一部分     引导作用

    ;//###########################################################################
    02 ;//
    03 ;// FILE:  DSP281x_CodeStartBranch.asm  
    04 ;//
    05 ;// TITLE: Branch for redirecting code execution after boot. 
    06 ;//
    07 ;//###########################################################################
    08 ;//
    09 ;//  Ver | dd mmm yyyy | Who  | Description of changes
    10 ;// =====|=============|======|===============================================
    11 ;//  1.00| 11 Sep 03   | L.H. | Updated based on D.A source to allow 
    12 ;//      |             |      | disabling the watchdog before branching to
    13 ;//      |             |      | the C init routine.  This is useful if the
    14 ;//      |             |      | watchdog is timing out before main() is reached.
    15 ;//###########################################################################  
    16   
    17   
    18 ***********************************************************************
    19   
    20 WD_DISABLE  .set    1       ;set to 1 to disable WD, else set to 0
    21   
    22     .ref _c_int00
    23   
    24 ***********************************************************************
    25 * Function: codestart section
    26 *
    27 * Description: Branch to code starting point
    28 ***********************************************************************
    29   
    30     .sect "codestart"
    31   
    32 code_start:
    33     .if WD_DISABLE == 1
    34         LB wd_disable       ;Branch to watchdog disable code
    35     .else
    36         LB _c_int00         ;Branch to start of boot.asm in RTS library
    37     .endif
    38   
    39 ;end codestart section
    40   
    41   
    42 ***********************************************************************
    43 * Function: wd_disable
    44 *
    45 * Description: Disables the watchdog timer
    46 ***********************************************************************
    47     .if WD_DISABLE == 1
    48   
    49     .text
    50 wd_disable:
    51     SETC OBJMODE        ;Set OBJMODE for 28x object code
    52     EALLOW              ;Enable EALLOW protected register access
    53     MOVZ DP, #7029h>>6  ;Set data page for WDCR register
    54     MOV @7029h, #0068h  ;Set WDDIS bit in WDCR to disable WD
    55     EDIS                ;Disable EALLOW protected register access
    56     LB _c_int00         ;Branch to start of boot.asm in RTS library
    57   
    58     .endif
    59   
    60 ;end wd_disable
    61   
    62   
    63   
    64     .end
    65       
    66 ; end of file CodeStartBranch.asm
  • bootloader 与CodeStartBranch有点类似物流系统与收货方的关系,bootloader 会根据不同的引导模式进行相应的操作。如果是flash与ram模式就会比较简单,bootloader会比较直接地引导到CodeStartBranch,而其他模式则会比较曲折,类似经过一些“中转站”。所以,CodeStartBranch应该只是bootloader 的最终入口,与bootloader机制并不具有严格的包含关系。当然,如果把概念放大一些,也是可以作为一部分的。看你的个人理解了。