This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
when I used C2000 Microcontroller Blockset in Simulink for Code generation,an error was occurred as follows:
"### Done Invoking postbuild tool "DWO Converter" ..."
"### Done Updating dependency files ..."
"### Successfully generated all binary outputs."
D:\ti\Matlab_2023_Examp28379D\Ledblinky_ert_rtw>exit /B 0
Download Executable to Hardware
Initiating the executable load sequence on the target hardware using TI Code Composer Studio.
SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
SLF4J: See www.slf4j.org/codes.html for further details.
js: Couldn't open file "D:\Program".
### Build procedure for Ledblinky aborted due to an error.
Build Summary
Top model targets built:
Model Action Rebuild Reason
=====================================================================
Ledblinky Failed Code generation information file does not exist.
0 of 1 models built (0 models already up to date)
Build duration: 0h 0m 25.019s
The following error occurred during deployment to your hardware board:
Error occurred during deployment to the hardware board. Check the 'Download Executable to Hardware' stage above for more details.
The configuration was set as:
the .out file is in the simulation path, but when i click on the Build, Deploy& Start. the error was appeared.