Part Number: TMS320F280025
外部电路有3路IO信号输入至DSP某3个IO口(例如GPIO11/GPIO12/GPIO13),现需要将GPIO11的上升沿同步EPWM1,GPIO12的上升沿同步EPWM2,GPIO13的上升沿同步EPWM3。
因280025提供了XBAR的INPUT5通过EXTSYNCIN1可以同步PWM1,INPUT6通过EXTSYNCIN2可以同步PWM2。
那么针对EPWM3,如何更好的将其配置为GPIO13上升沿同步?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025
外部电路有3路IO信号输入至DSP某3个IO口(例如GPIO11/GPIO12/GPIO13),现需要将GPIO11的上升沿同步EPWM1,GPIO12的上升沿同步EPWM2,GPIO13的上升沿同步EPWM3。
因280025提供了XBAR的INPUT5通过EXTSYNCIN1可以同步PWM1,INPUT6通过EXTSYNCIN2可以同步PWM2。
那么针对EPWM3,如何更好的将其配置为GPIO13上升沿同步?
可以通过ePWM-BAR实现上升沿触发同步信号。
input-bar->epwm-bar产生trip信号到epwm的DC子模块,子模块触发DCEVT1事件最终产生同步输出信号到TB子模块,这样就可以进行同步了。