This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRINSPIN: 关于套件的低速配置以及0速的相关问题

Part Number: TMDSHVMTRINSPIN

您好,TI 的工程师们

我是一个新手,目前正在使用TMDSHVMTRINSPIN F28069来控制永磁同步电机。目前我用的是lab05c,我目前有几个问题想请教一下:

1.低速问题:我的电机可以实现额定3000rpm的适配器,目前我在ccs中测试50rpm,100rpm,500rpm和1000rpm效果很好。但低于50rpm就会出现给不上的情况。我在表达式窗口中在gMotorVars.SpeedRef_krpm(IQ24)给0,他没有变化,是默认100rpm。但是我给10的情况下,电机就会出现一抖一抖的情况,他参考速度会瞬间跳变到100rpm,然后有瞬间跳回去。请问这个默认值100rpm(1677721)是在哪里设置的?如果让电机停止的的话可以给0速实现吗?低速情况下出现这种情况是什么原因呢?

2.我想实现电机抱死功能(就像刹车一样),可以在代码来施加固定的电流来锁死转子吗?

3,我还想获得底部的位置信息,我目前利用EST_getSpeed_krpm来获得当前速度,之后算成角速度,最后得到角位移。在角速度得到角位移的过程中需要获得时间才能得到角位移。为了保证换算代码的角位移和实际电机运转的角位移保持一致,请问这个时间如何设定呢?

4.请问StopSpeedRef_krpm代表的含义是什么呢

谢谢工程师们,祝你们生活顺利,一帆风顺

此致

刘