你好:
在用C2PROG对TMS320F28015进行串口烧写时,DSP不响应。硬件上已经设置为SCI烧写模式(GPIO34=0,GPIO18=1),使用SDFLASH软件能够通过串口烧写且运行正常,但是由于各种原因,需要用C2PROG烧写,使用C2PROG就出现下面的错误:
*** PLEASE RESET TARGET IN SCI BOOT-LOADER MODE ***
Pinging target... no response!
通过示波器测量DSP的串口接收引脚(GPIO28),其接收引脚出现大概10个左右如下图的波形,波形的形状都是一样的,不一样的是高低电平的宽度不一样,但是DSP的串口输出引脚(GPIO29)一直无输出,DSP不响应,请问是怎么回事啊??非常感谢大侠能帮忙解决!!