This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP 28335 死机后不能复位



已经量产的板子,最近发现有这样的情况,在外部干扰下,DSP 28335死机,不能正确复位。

具体情况是28335死机时,MAX705提供复位信号经过CPLD给28335的80脚nXRS。复位信号时约为200ms的低电平脉冲,在复位时测量XA12、XA13、XA15是高电平脉冲约230ms,XA14一直是高电平。这时不管是手动按键复位还是MAX705看门狗复位都不行,只有断电重启才可以正常复位。

对比了一下正常情况下MAX705提供的复位重启,和XA12、XA13、XA14、XA15的信号和上诉一样,可是28335可以正常复位启动。