dsp2812 flash 固化后,在0x3d8000地址上已经改动了,为什么每次只有插上仿真器才能运行,试了好多天了,就有一次莫名其妙好使了,不插仿真器也好使,现在怎么弄都不行?急求。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dsp2812 flash 固化后,在0x3d8000地址上已经改动了,为什么每次只有插上仿真器才能运行,试了好多天了,就有一次莫名其妙好使了,不插仿真器也好使,现在怎么弄都不行?急求。谢谢。
我的是学习开发板,硬件应该没问题,我昨天晚上也没弄啥,今天早上莫名其妙的就好使了。但是我重新下载以后又不好使了。真是奇怪了。
weihang gao 说:我的是学习开发板,硬件应该没问题,我昨天晚上也没弄啥,今天早上莫名其妙的就好使了。但是我重新下载以后又不好使了。真是奇怪了。
那可以实际测量一下MP/MC#引脚,看一下到底是不是低电平
如果是低电平,那应该是可以启动的。
不知道你的程序是什么样的,你是不是应该使用一个最简单的小程序来测试,比如点亮一个LED来看看会不会有问题。
还是不行,真是莫名其妙的,
MEMORY /* Program Memory */
{
PAGE 0 :
FLASH : origin = 0x3D8000, length = 0x01FF80 /* on-chip FLASH */
BEGIN : origin = 0x3F7FF6, length = 0x000002
ROM : origin = 0x3FF000, length = 0x000FC0
RESET : origin = 0x3FFFC0, length = 0x000002
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of Boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
RAML0 : origin = 0x008000, length = 0x001000
PAGE 1 :
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */
DEV_EMU : origin = 0x000880, length = 0x000180 /* device emulation registers */
PIE_VECT : origin = 0x000D00, length = 0x000100 /* PIE Vector Table */
FLASH_REGS : origin = 0x000A80, length = 0x000060 /* FLASH registers */
CSM : origin = 0x000AE0, length = 0x000010 /* code security module registers */
XINTF : origin = 0x000B20, length = 0x000020 /* external interface registers */
CPU_TIMER0 : origin = 0x000C00, length = 0x000008 /* CPU Timer0 registers */
CPU_TIMER1 : origin = 0x000C08, length = 0x000008 /* CPU Timer1 registers */
CPU_TIMER2 : origin = 0x000C10, length = 0x000008 /* CPU Timer2 registers */
PIE_CTRL : origin = 0x000CE0, length = 0x000020 /* PIE control registers */
ECANA : origin = 0x006000, length = 0x000040 /* eCAN control and status registers */
ECANA_LAM : origin = 0x006040, length = 0x000040 /* eCAN local acceptance masks */
ECANA_MOTS : origin = 0x006080, length = 0x000040 /* eCAN message object time stamps */
ECANA_MOTO : origin = 0x0060C0, length = 0x000040 /* eCAN object time-out registers */
ECANA_MBOX : origin = 0x006100, length = 0x000100 /* eCAN mailboxes */
SYSTEM : origin = 0x007010, length = 0x000020 /* System control registers */
SPIA : origin = 0x007040, length = 0x000010 /* SPI registers */
SCIA : origin = 0x007050, length = 0x000010 /* SCI-A registers */
XINTRUPT : origin = 0x007070, length = 0x000010 /* external interrupt registers */
GPIOMUX : origin = 0x0070C0, length = 0x000020 /* GPIO mux registers */
GPIODAT : origin = 0x0070E0, length = 0x000020 /* GPIO data registers */
ADC : origin = 0x007100, length = 0x000020 /* ADC registers */
EVA : origin = 0x007400, length = 0x000040 /* Event Manager A registers */
EVB : origin = 0x007500, length = 0x000040 /* Event Manager B registers */
SCIB : origin = 0x007750, length = 0x000010 /* SCI-B registers */
MCBSPA : origin = 0x007800, length = 0x000040 /* McBSP registers */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations. */
}
/*------------------------------------------*/
/*描述:设置堆栈值 */
/*------------------------------------------*/
-stack 400
/*------------------------------------------*/
/*描述:通过SECTION伪指令来分配段到存储空间 */
/*------------------------------------------*/
SECTIONS
{
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS, PAGE = 0, TYPE = DSECT
.cinit : > FLASH, PAGE = 0
.text : > FLASH, PAGE = 0
codestart : > BEGIN, PAGE = 0
ramfuncs: LOAD=FLASH, PAGE=0
RUN=RAML0,PAGE=0
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart)
.const : > FLASH, PAGE = 0
.econst : > FLASH, PAGE = 0
.data2 : > RAMM1, PAGE = 1
.stack : > RAMM0, PAGE = 1
.bss : > RAML1, PAGE = 1
.ebss : > RAML1, PAGE = 1
.sysmem : > RAMH0, PAGE = 1
.esysmem : > RAMH0, PAGE = 1
/* Allocate IQ math areas: */
IQmath : > FLASH, PAGE = 0 /* Math Code */
IQmathTables : > ROM, PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
PieVectTableFile : > PIE_VECT, PAGE = 1
/*** Peripheral Frame 0 Register Structures ***/
DevEmuRegsFile : > DEV_EMU, PAGE = 1
FlashRegsFile : > FLASH_REGS, PAGE = 1
CsmRegsFile : > CSM, PAGE = 1
XintfRegsFile : > XINTF, PAGE = 1
CpuTimer0RegsFile: > CPU_TIMER0, PAGE = 1
CpuTimer1RegsFile: > CPU_TIMER1, PAGE = 1
CpuTimer2RegsFile: > CPU_TIMER2, PAGE = 1
PieCtrlRegsFile : > PIE_CTRL, PAGE = 1
/*** Peripheral Frame 1 Register Structures ***/
ECanaRegsFile : > ECANA, PAGE = 1
ECanaLAMRegsFile : > ECANA_LAM PAGE = 1
ECanaMboxesFile : > ECANA_MBOX PAGE = 1
ECanaMOTSRegsFile: > ECANA_MOTS PAGE = 1
ECanaMOTORegsFile: > ECANA_MOTO PAGE = 1
/*** Peripheral Frame 2 Register Structures ***/
SysCtrlRegsFile : > SYSTEM, PAGE = 1
SpiaRegsFile : > SPIA, PAGE = 1
SciaRegsFile : > SCIA, PAGE = 1
XIntruptRegsFile : > XINTRUPT, PAGE = 1
GpioMuxRegsFile : > GPIOMUX, PAGE = 1
GpioDataRegsFile : > GPIODAT PAGE = 1
AdcRegsFile : > ADC, PAGE = 1
EvaRegsFile : > EVA, PAGE = 1
EvbRegsFile : > EVB, PAGE = 1
ScibRegsFile : > SCIB, PAGE = 1
McbspaRegsFile : > MCBSPA, PAGE = 1
/*** Code Security Module Register Structures ***/
CsmPwlFile : > CSM_PWL, PAGE = 1
}
这是我的CMD文件,
有人告诉
cmd用官方的就好,别乱改,flash中仿真可以,就应该不是它的问题。