This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!请问C2000系列的MCU有供电及输入出端口均为5V的型号吗?如果有的话,麻烦您给推荐几个型号。谢谢!
应该没有
感谢您的回复!请问其他系列的MCU是不是也没有5V的?因为我的芯片用在汽车领域,之前用的一款3.3V的,感觉很不方便。
祝好!
现在好像很少用5V的吧,除了51系列的单片机。
感觉不方便应该也就是引脚电平吧,有时可以用cpld进行转换,最好还是用3.3V,比较通用。