This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000v6.2 和 C2000v6.5编译器问题



请问各位学者,我在电脑上安装了CCS5.4,打开某工程时候报错,信息为:please install the c2000v6.2 compiler before inporting this progect ;

然后我又安装了CCS6.0,打开同样工程时候还是报错,信息为:please install the c2000v6.5 compiler before inporting this progect ;

请问这个问题该如何解决呢?

  • 相关解答

    Which specific version of CCSv5 are you using? Are you sure the project you are importing is a "CCS project" and not a standard Eclipse project?

    Are you able to import the same project through the CCS GUI rather than via command line?

    What versions of compilers do you see listed under Window->Preferences->Code Composer Studio->Build->Compilers? CCS 5.2.x should already have compiler v6.1.0 for C2000 and what that version I wouldn't expect this error to appear.

  • 建议你先安装6.2和6.4.4的编译器,以下是编译器地址:

    http://software-dl.ti.com/codegen/non-esd/downloads/download.htm#C2000

  • hi  囧

    我想下载C2000v6.2,TI回复需要审核,可是我真的急用,在网上其他地方也没找到,能帮我下载一下吗,谢谢你啦!  1229789893@qq.com   或回复在帖子里也行   再次感谢

  • hi囧  不用了   早上申请时换了个国家    下载下来了    谢谢