VDDIO接的是3.3V电平
另外一个问题:EPWMx的A和B之间的相差能否设定为某个值,例如90度?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VDDIO接的是3.3V电平
另外一个问题:EPWMx的A和B之间的相差能否设定为某个值,例如90度?
但是他们相对于同步时钟的相差,A和B是共用一个相位寄存器的,那这样A相对B是不能设相位差的,也就是说AB相位时钟是相同的是吧
因为我现在想发生一个相差90度的PWM波,
看来只能通过不同的ePWMx模块,例如ePWM1A和ePWM2A
不能通过同一个ePWMxA和ePWMxB了是吧