This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: SCI发送数据出现偶发丢帧

Part Number: TMS320F28374S


测试工况:28374s与多3块2800157芯片进行SCI转485通讯时偶发丢帧,28374s为主控,2800157均为从控,轮询发送回复,波特率19200,发送时间50ms、100ms均测试,500ms测试不丢帧

测试现象:监测DSP端口的RX和TX引脚波形出现偶发丢帧,CH1为TX引脚波形,CH2为RX引脚波形,发送一帧回复一帧,中间发送引脚存在两处丢帧,引起RX不回复。

初步定位的两个现象:

(1)28374s芯片与三块2800157芯片待机通讯均无丢帧,28374s设备接入AC电后会间歇性丢帧,且AC源给非常小的电压仍会丢帧(接近0V),通过此现象可能更接近于硬件问题。

(2)上AC电待机但三块2800157芯片不进行回复,28374s只发送,多块2800157不进行回复,也不会造成28374s发送丢失,通过此现象可能更接近于软件问题。

因此想请教一下,软件上是否还存在一些其他的因素会导致28374s自身发送丢失(屏蔽掉所有其他无法的中断程序和任务均不会影响丢帧现象的产生),或硬件上有什么因素会影响SCI通讯丢帧?