This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TI开发板(TMDS2MTRPFCKIT)用于控制2个永磁同步电机



前段时间购买了一个TI官网的开发板(TMDS2MTRPFCKIT(F28035))用于控制两个电机,但是在调试过程(LEVEL 1)中出现一些问题:

1. 使用的是CCS5.5版本,在debug界面,选择debug界面的中的“Enable real-time mode”时(严格按照此开发板的使用说明),同时选中continue refresh时,点击“运行”按钮时,出现如下错误,并且按照它的提示,选择“Rude Retry“时程序却不能运行。

Trouble Reading Register PC:

(Error -1142 @ 0x0)

Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.

(Emulation package 5.1.232.0)

2. 另外,开发板自带的GUI程序也不能使用。

请问这些问题怎么解决?麻烦大家帮忙分析一下。