This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于F28M35的SSI模块设置问题



目前我设置完SSI的模块后,使用SSIDataPut(SSI2_BASE,0x0f);发送数据,发现GPIO口无任何响应,示波器也无法检测到信号。

请问是否哪里设置错误,希望得到指正,我的芯片外部时钟频率为25M。谢谢!

函数是这样的:

void InitGpio(){
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL) |= GPIO_PCTL_PB0_SSI2TX |GPIO_PCTL_PB1_SSI2RX |GPIO_PCTL_PB2_SSI2CLK |GPIO_PCTL_PB3_SSI2FSS; //设置PB0为SSI2TX ,PB1为_SSI2RX,PB2为SSI2CLK ,PB3为SSI2FSS

SSIConfigSetExpClk(SSI2_BASE,SysCtlClockGet(25000000),SSI_FRF_MOTO_MODE_3,SSI_MODE_MASTER,2000000,8);

SSIEnable(SSI2_BASE);
SSIDataPut(SSI2_BASE,0x0f); //发送一个数据

}

int main(void) {
//Disable Protection
unsigned char ledshow[6],i,key;

HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;

// Sets up PLL, M3 running at 100MHz and C28 running at 100MHz
SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0x8) |
SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_1|SYSCTL_XCLKDIV_4);

memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

FlashInit();
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG1);
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG0);
IntMasterEnable();

InitGpio();//设置ssi模式并发送数据
while(1){

}

}

  • 你选择SSI2在PB的GPIO口,需要配置GPIO的外设模式为alternate peripheral模式。

    需要设置寄存器GPIOAPSEL。
    建议你调用如下的函数:

    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
    GPIOPinConfigure(GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0TX);

    // Configure the GPIO settings for the SSI pins. This function also gives
    // control of these pins to the SSI hardware. Consult the data sheet to
    // see which functions are allocated per pin.
    // The pins are assigned as follows:
    // PA5 - SSI0Tx
    // PA4 - SSI0Rx
    // PA3 - SSI0Fss
    // PA2 - SSI0CLK
    // TODO: change this to select the port/pin you are using.
    GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |
    GPIO_PIN_2);

    Eric