This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问上电以后要不要CPU1发个什么命令给CPU2,还是CPU2一上电就自动运行,程序是烧到FLASH里面的,CPU1的可以运行,CPU2的运行不了
需要给CPU2引导命令。
#ifdef _STANDALONE
#ifdef _FLASH
// Send boot command to allow the CPU02 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
// Send boot command to allow the CPU02 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif
你参考controlSUITE中例程:C:\ti\controlSUITE\device_support\F2837xD\v150\F2837xD_examples_Dual\blinky_dc\cpu01
Eric
Ti 工程师 好。
我也遇到了该问题,我是将工程直接从C:\ti\controlSUITE\device_support\F2837xD\v150\F2837xD_examples_Dual\blinky_dc 导出CUP1 和CUP2工程, 配置是cup1工程是:CUP1_FLASH_DEBUG [ACTIVE] ,cpu2工程是:CUP2_FLASH [ACTIVE],在线仿真同时将程序烧写到CUP1和CPU2 FLASH中,退出仿真,断电上电,CUP1 可以工作(28377D 开发板LD2闪烁),CUP2不可以工作(28377D 开发板LD3不闪烁)。仿真下CUP1和CPU2都工作的(LD2闪烁,LD3闪烁)
寻求帮助,该问题已经搞了好几天了,急。谢谢
上个帖子不是说了吗,你要给CPU2启动命令。需要让代码IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);参与编译。
你可以直接在main前面 #define STANDALONE 1
#define FLASH 1
#ifdef _STANDALONE
#ifdef _FLASH
// Send boot command to allow the CPU2 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
// Send boot command to allow the CPU2 application to begin execution
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif