This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于F28069ADC采样的问题



各位好,我在做无刷电机的FOC驱动,使用的是F28069,但是在采样电流的过程中,ADC的的采集不是很准确,上下跳动得挺厉害得,有0.1V的误差,再根据0.02mΩ的采样电阻,7.5的放大倍数,那么一计算就有了0.6A的误差了。ADC是由PWM触发的,在下桥臂开通的情况下采样,在ADC中断中读取ADC值,也使用了一阶滤波算法,采集的数据还是跳动很厉害。请问如何可以提高ADC的精度和稳定性?另外一个问题是,FOC驱动方式,需不需要高的电流精度值?谢谢

  • 首先    你的采样电阻   阻值精度能到多少     

    其次   ADC采样的数据肯定是有些偏差的       12位的    就当10位用吧

    加上电机套件母线电流的波动是很大的     如果是PWM波触发ADC  

    建议选择不同的触发时刻   看看效果是否会好些