使用芯片F28M35H52C1,需要在C28核代码中植入擦写程序,擦写区域是C28的全部FLASH,用的是F021_API_C28x_FPU32.lib库函数,并且在程序中使用pragma将操作FLASH的代码都指定到了ram区。但是在F021_API_C28x_FPU32.lib库函数中调用了rts2800_fpu32.lib库中的LL$$OR,并且无法用pragma将rts2800_fpu32.lib指定到ram区,在擦写rts2800_fpu32.lib所在区域的FLASH时就会产生错误。以前用F28335时也做过类似的代码,也是使用的TI提供的FLASH库函数,就没有这种问题。请问怎么解决?