This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.5导入工程的问题,谢谢



工程师:

             你好。

             我电脑上先后安装了CCS6.0 ,CCS5.5。 最开始使用Instapin中的projet 5b 程序使用CCS6.0 打开的,后来因为仿真器的原因使用CCS5.5。不过文件在CCS6.0可以打开,在CCS5.5中打不开了,但是CCS5.5还是可以打开Instaspin中的其他工程。

             我想咨询下,是不是在CCS6.0中打开保存后的工程就不能在CCS5.5中打开了?可不可以将工程从CCS6.0的版本降低到CCS5.5可以降低的版本?

best regards

附:下面的导入CCS5.5提示的错误

See details below. 
Error: Import failed for project ' XXX' because its meta-data cannot be interpreted. Please contact support.