This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CNTL-2P2Z 和PID



CNTL-2P2Z

U[n]=A1*U[n-1]+A2*U[n-2]+B0*e[n]+B1*e[n-1]+B0*e[n-2]

PID

U[n]=U[n-1]+(Kp+Ki+Kd)*e[n]+(-Kp-2*Kd)*e[n-1]+Kd*e[n-2]

B0=Kp+Ki+Kd

B1=-Kp-2*Kd

B2=Kd

A2=0

A1=1

但是在Ti给的开发套件程序里,设定

B1=Ki-Kp-2*Kd  这是怎么回事?

另外:在Ti的开发套件程序里,设定:

CNTL-2P2Z的系数按照下列Q值格式,即Q26的格式

b2= _IQ26(0.35);
 b1 = _IQ26(-1.45);
 b0 _IQ26(1.33);
 a2= _IQ26(-0.23);
 a1 = _IQ26(1.23);

但是在PID转换成CNTL-2P2Z的系数后,出现了b2,b1,b0的格式是Q16,但是a1和a2的格式却是Q26的格式

b2 = _IQ16(Dgain);
b1 = _IQ16(Igain - Pgain - Dgain - Dgain);
b0 = _IQ16(Pgain + Igain + Dgain);
a2 = _IQ26(0.0);
a1 = _IQ26(1.0);

CNTL-2P2Z的汇编程序如下:

CNTL_2P2Z_INIT .macro n
;=============================
; allocate memory space for data & terminal pointers
_CNTL_2P2Z_Ref:n: .usect  "CNTL_2P2Z_Section",2,1,1  ; reference input terminal
_CNTL_2P2Z_Fdbk:n: .usect  "CNTL_2P2Z_Section",2,1,1  ; feedback input terminal
_CNTL_2P2Z_Out:n: .usect  "CNTL_2P2Z_Section",2,1,1  ; output terminal
_CNTL_2P2Z_Coef:n: .usect  "CNTL_2P2Z_Section",2,1,1  ; coefficients & saturation limits (14 words)
_CNTL_2P2Z_DBUFF:n: .usect  "CNTL_2P2Z_Section",10,1,1  ; internal Data BUFF

; publish terminal pointers for access from the C environment
  .def  _CNTL_2P2Z_Ref:n:
  .def  _CNTL_2P2Z_Fdbk:n:
  .def  _CNTL_2P2Z_Out:n:
  .def  _CNTL_2P2Z_Coef:n:
  .def  _CNTL_2P2Z_DBUFF:n:

; set terminal pointers to ZeroNet
  MOVL XAR2, #ZeroNet
  MOVW DP, #_CNTL_2P2Z_Ref:n:
  MOVL @_CNTL_2P2Z_Ref:n:, XAR2
  MOVW DP, #_CNTL_2P2Z_Fdbk:n:
  MOVL @_CNTL_2P2Z_Fdbk:n:, XAR2
  MOVW DP, #_CNTL_2P2Z_Out:n:
  MOVL @_CNTL_2P2Z_Out:n:, XAR2

; zero data buffer
  MOVW DP, #_CNTL_2P2Z_DBUFF:n:
  MOVL  XAR2,#_CNTL_2P2Z_DBUFF:n:
  RPT  #9  ; 10 times
 || MOV  *XAR2++, #0
 
  .endm

;----------------------------------------------------------------------------------
;=============================
CNTL_2P2Z .macro n
;=============================
; set up address pointers
  MOVW DP, #_CNTL_2P2Z_Ref:n:
  MOVL  XAR0, @_CNTL_2P2Z_Ref:n:  ; net pointer to Ref (XAR0)
  MOVW DP,#_CNTL_2P2Z_Fdbk:n:
  MOVL    XAR1, @_CNTL_2P2Z_Fdbk:n:  ; net pointer to Fdbk (XAR1)
  MOVW DP,#_CNTL_2P2Z_DBUFF:n:
  MOVL XAR4, #_CNTL_2P2Z_DBUFF:n:  ; pointer to the DBUFF array (used internally by the module)
  
; calculate error (Ref - Fdbk)
  MOVL ACC, *XAR0      ; ACC = Ref (Q24) = Q(24)
  SUBL ACC, *XAR1         ; ACC = Ref(Q24) - Fdbk(Q24)= error(Q24)
  LSL     ACC, #6       ; Logical left shift by 6,  Q{24}<<6 -> Q{30}
;store error in DBUFF
  MOVL *+XAR4[4], ACC     ; e(n) = ACC = error Q{30}  
  
  MOVW DP,#_CNTL_2P2Z_Out:n:
  MOVL    XAR2, @_CNTL_2P2Z_Out:n:  ; net pointer to Out (XAR2)
  MOVW DP,#_CNTL_2P2Z_Coef:n:
  MOVL    XAR3, @_CNTL_2P2Z_Coef:n:  ; net pointer to Coef (XAR3)
  ZAPA  
; compute 2P2Z filter
  MOV  AR0,#8
  MOVL XT, *+XAR4[AR0]     ; XT  = e(n-2)
  QMPYL P, XT, *XAR3++     ; P   = e(n-2)Q30*B2{Q26} = I8Q24
  MOVDL XT, *+XAR4[6]     ; XT  = e(n-1), e(n-2) = e(n-1)
  QMPYAL P, XT, *XAR3++      ; P   = e(n-1)Q30*B1{Q26} = Q24, ACC=e(n-2)*B2
  MOVDL XT, *+XAR4[4]      ; XT  = e(n), e(n-1) = e(n)
  QMPYAL P, XT, *XAR3++      ; P   = e(n)Q30*B0{Q26}= Q24, ACC = e(n-2)*B2 + e(n-1)*B1
  MOVL XT,*+XAR4[2]     ; XT  = u(n-2)
  QMPYAL P, XT, *XAR3++     ; P   = u(n-2)*A2, ACC = e(n-2)*B2 + e(n-1)*B1 + e(n)*B0
  MOVDL XT,*+XAR4[0]      ; XT  = u(n-1), u(n-2) = u(n-1)
  QMPYAL P, XT, *XAR3++      ; P   = u(n-1)*A1, ACC = e(n-2)*B2 + e(n-1)*B1 + e(n)*B0 + u(n-2)*A2
  ADDL ACC, @P       ; ACC = e(n-2)*B2 + e(n-1)*B1 + e(n)*B0 + u(n-2)*A2 + u(n-1)*A1

; scale u(n):Q24, saturate (max>u(n)>min0), and save history
  
  MINL ACC, *XAR3++      ; saturate to < max (Q24)
  MAXL ACC, *XAR3       ; saturate to > min (Q24)

; write controller result to output terminal (Q24)
  MOVL *XAR2, ACC      ; output control effort to terminal net

; Convert the u(n) to Q30 format and store in the data buffer
  LSL     ACC, #6       ; Logical left shift by 6, Q{24}<<6 -> Q{30}
  MOVL *XAR4, ACC      ; u(n-1) = u(n) = ACC

  .endm

问题:

b2 = _IQ16(Dgain);
b1 = _IQ16(Igain - Pgain - Dgain - Dgain);
b0 = _IQ16(Pgain + Igain + Dgain);
a2 = _IQ26(0.0);
a1 = _IQ26(1.0);
系数 a1和a2的格式不是Q16的话,不是相当于

b2 = _IQ16(Dgain>>10);
b1 = _IQ16((Igain - Pgain - Dgain - Dgain)>>10);
b0 = _IQ16((Pgain + Igain + Dgain)>>10);
a2 = _IQ26(0.0);
a1 = _IQ26(1.0);

这样相当于PID的公式变为:

U[n]=1024*U[n-1]+(Kp+Ki+Kd)*e[n]+(-Kp-2*Kd)*e[n-1]+Kd*e[n-2]   ???

希望给予解答,谢谢!

  • 帖子中,有处写错了, 现修改如下:

    问题:

    b2 = _IQ16(Dgain);

    b1 = _IQ16(Igain - Pgain - Dgain - Dgain);

    b0 = _IQ16(Pgain + Igain + Dgain);

    a2 = _IQ26(0.0);

    a1 = _IQ26(1.0);

    系数 a1和a2的格式不是Q16的话,不是相当于

    b2 = _IQ26(Dgain>>10);

    b1 = _IQ26((Igain - Pgain - Dgain - Dgain)>>10);

    b0 = _IQ26((Pgain + Igain + Dgain)>>10);

    a2 = _IQ26(0.0);

    a1 = _IQ26(1.0);

    这样相当于PID的公式变为:

    U[n]=1024*U[n-1]+(Kp+Ki+Kd)*e[n]+(-Kp-2*Kd)*e[n-1]+Kd*e[n-2]   ???

    希望给予解答,谢谢!

  • 有人能帮忙解决下吗?

  • 求教,

    TI 的PFC+ACI套件,实测发现在交流220输入,直流390V输出时,PF值只有80%,有没有好的解决办法?

    如果调整PID系数的话,是只调整电流环还是要电流环电压环一起调整?有没有参考的把参数?

    谢谢