This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C123G 与HC-06蓝芽模组通讯

Other Parts Discussed in Thread: ENERGIA


各位前辈,晚辈是使用TI MCU的新手,从前有一些Arduino的经验。从前晚辈曾经使用Arduino Uno + HC-06蓝芽模组与手机的Android沟通。使用以下coding:
 

/*
  Sends sensor data to Arduino
  (needs SensorGraph and Amarino app installed and running on Android)
*/
 
#include <MeetAndroid.h>

MeetAndroid meetAndroid;

float temp;
void setup()  
{
  // use the baud rate your bluetooth module is configured to
  // not all baud rates are working well, i.e. ATMEGA168 works best with 57600
  Serial.begin(115200);
 

}

void loop()
{
  double C1 = analogRead(A0);
 
  int vol =5*1000 - C1*1000*5/1024;
 
 
 
  if (vol == temp)
  { temp == vol;
  }
  else
  {

  meetAndroid.receive(); // you need to keep this in your loop() to receive events
 
  // read input pin and send result to Android
  meetAndroid.send(vol);
 
  // add a little delay otherwise the phone is pretty busy
  delay(300);
  }

我想请教的是能否用DK-TM4C123G做到相同效果? 而PIN的RX TX连接又是怎样?由於晚辈第一次使用TI ,PIN的接合还是不熟悉。使用Energia 编程又是否和以上coding 一样? 还望各位前辈指教