This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 printf问题



您好:

我在ti官方网站,看到ccsv4对printf的实现如下

add_device("uart", _SSA, uart_open, uart_close, uart_read, uart_write, uart_lseek, uart_unlink, uart_rename);

fopen("uart","w");

freopen("uart:", "w", stdout); // redirect stdout to uart

setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout

printf("^_^\r\n");

但发现printf有时候带参数时,参数无法输出的现象。

谢谢

  • 我试了一下,没能重复这个问题。

    建议楼主把CCS升级到最新版本再试,楼主用的是哪款芯片,程序是怎么写的?

  • 感谢Forrest的回答, 下面是我的初始化函数

    使用CCS4.2 和CCS4.12仿似都不行 芯片是F28335

    void bsp_InitUart(void)

    {

    //the next 4 lines are from ti

    add_device("uart", _SSA, uart_open, uart_close, uart_read, uart_write, uart_lseek, uart_unlink, uart_rename);

    fopen("uart","w");

    freopen("uart:", "w", stdout); // redirect stdout to uart

    setvbuf(stdout, NULL, _IONBF, 0); // turn off buffering for stdout

    printf("^_^\r\n");  

    }

    int uart_open(const char *path, unsigned flags, int llv_fd)

    {

    uint16_t baudrate;

    #ifdef SCI_PORT_A

    InitSciaGpio();

    #elif defined(SCI_PORT_B)

    InitScibGpio();

    #else

    InitScicGpio();

    #endif

       ScibRegs.SCIFFTX.all=0xE040;

       ScibRegs.SCIFFRX.all=0x204f;

       ScibRegs.SCIFFCT.all=0x0;

    SCI.SCICCR.all =0x0007;   // 1 stop bit,  No loopback

                                      // No parity,8 char bits,

                                      // async mode, idle-line protocol

    SCI.SCICTL1.all = 0x0003;  // enable TX, RX, internal SCICLK,

                                      // Disable RX ERR, SLEEP, TXWAKE

    SCI.SCICTL2.bit.TXINTENA = 0;

    SCI.SCICTL2.bit.RXBKINTENA = 0;

    baudrate = SCI_PRD;

    baudrate = (baudrate >> 8);

    SCI.SCIHBAUD    = baudrate;  // 9600 baud @LSPCLK = 37.5MHz.

    baudrate = SCI_PRD;

    baudrate = (baudrate & 0x00FF);

    SCI.SCILBAUD    = baudrate;

    SCI.SCIFFRX.all = 0x0001;

    SCI.SCICTL1.all = 0x0023;  // Relinquish SCI from Reset

       SCI.SCIFFTX.bit.TXFIFOXRESET=1;                              

       SCI.SCIFFRX.bit.RXFIFORESET=1;

    }

    int uart_close(int dev_fd){return ;}

    int uart_read(int dev_fd, char *buf, unsigned count)

    {

      //while(count--)

      {

        while(SCI.SCIFFRX.bit.RXFFST == 0) { } // wait for XRDY =1 for empty state

          // Get character

          *buf++ = (char)SCI.SCIRXBUF.all;

        }

    return count;

    }

    int uart_write(int dev_fd, const char *buf, unsigned count)

    {

       //while(count--)

       {

    while (SCI.SCIFFTX.bit.TXFFST != 0) {}

        SCI.SCITXBUF = *buf++;

       }

    return count;

    }

    off_t uart_lseek(int dev_fd, off_t offset, int origin){return ;}

    int uart_unlink(const char *path){return ;}

    int uart_rename(const char *old_name, const char *new_name){return ;}

    谢谢

  • 补充:

    printf("baudrate is %d\n",9600);  没问题

    baudrate = 9600;

    printf("baudrate is %d\n",baudrate); 不可以 正确输出baudrate is 9600

    谢谢

  • Forrest 你好,我的代码已贴出,能否给贴一下你的 给look一下,thanks

  • 我试了一下,可以的。请看一下下面链接,所有要注意的里面都有说:

    processors.wiki.ti.com/.../Tips_for_using_printf

  • 你好,谢谢你的回答,呵呵,之前我对printf重定向时参考的就是这个文档,也许什么地方没注意到,我再仔细看看,实验一下把。谢谢