This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 DSP中断优先级



1.首先要找到文件,DSP281x_SWPrioritizedDefaultIsr.c 和DSP281x_SWPrioritizedIsrLevels.h加载到你的程序当中。
2.在DSP281x_SWPrioritizedIsrLevels.h文件中先设置中断组的优先级级别。其中:0表示不使用;1表示优先级最高;16表示优先级最低;
比如:我设置第9组优先级最高,第3组次之,第2,4,6组优先级为第三。其他以此类推。0表示不用。
#define INT1PL 4 // Group1 Interrupts (PIEIER1)
#define INT2PL 3 // Group2 Interrupts (PIEIER2)
#define INT3PL 2 // Group3 Interrupts (PIEIER3)
#define INT4PL 3 // Group4 Interrupts (PIEIER4)
#define INT5PL 4 // Group5 Interrupts (PIEIER5)
#define INT6PL 3 // Group6 Interrupts (PIEIER6)
#define INT7PL 0 // reserved
#define INT8PL 0 // reserved
#define INT9PL 1 // Group9 Interrupts (PIEIER9)
#define INT10PL 0 // reserved
#define INT11PL 0 // reserved
#define INT12PL 0 // reserved
#define INT13PL 5 // XINT3
#define INT14PL 5 // INT14 (TINT2)
#define INT15PL 5 // DATALOG
#define INT16PL 5 // RTOSINT
3.级中断设置好以后,我们就要设置每一组里的中断优先级级别。其中:0表示不用;1表示优先级最高;8表示优先级最低;
以第9组为例说明:其中,ECAN0INTA优先级最高;ECAN1INTA为第2,SCIRXINTA为第3。其他自己数。
#define G91PL 3 // SCIRXINTA (SCI-A)
#define G92PL 5 // SCITXINTA (SCI-A)
#define G93PL 6 // SCIRXINTB (SCI-B)
#define G94PL 4 // SCITXINTB (SCI-B)
#define G95PL 1 // ECAN0INTA (ECAN-A)
#define G96PL 2 // ECAN1INTA (ECAN-A)
#define G97PL 0 // reserved
#define G98PL 0 // reserved
4.由上可知所有组里第9组优先级最高,第9组中ECAN0INTA(G95PL)优先级最高。优先级设置好后到 DSP281x_SWPrioritizedDefaultIsr.c
文件中找到相应的函数。我这里就拿ECAN0INTA(ECAN-A)来作为例子说明;
这个中断对应的函数为(DSP281x_SWPrioritizedDefaultIsr.c 文件里可以找到)如下:
//---------------------------------------------------------------------------
// eCAN-A Default ISRs:
//
// Connected to PIEIER9_5 (use MINT9 and MG95 masks):
#if (G95PL != 0)
interrupt void ECAN0INTA_ISR(void) // eCAN-A
{
// Set interrupt priority:
volatile Uint16 TempPIEIER = PieCtrlRegs.PIEIER9.all;

/* 以下表示,大于第9组中断级别的中断使能,小于第9组中断级别的中断不使能*/
IER |= M_INT9;
IER &= MINT; // Set "global" priority

/*优先级大于第9组中第5个中断的中断使能,否则不使能*/
PieCtrlRegs.PIEIER9.all &= MG95; // Set "group" priority

PieCtrlRegs.PIEACK.all = 0xFFFF; // Enable PIE interrupts

EINT; //全局中断使能,但因为此中断优先级最高,所以其他一般中断不能打断它

// Insert ISR Code here.......
CAN_ISR(); //你自己定义的中断处理程序,在此程序中写你自己的代码;
// Restore registers saved:
DINT; //关中断
PieCtrlRegs.PIEIER9.all = TempPIEIER;
}
#endif

问题:

1.为什么要在中断函数的结尾处关总中断?即执行 DINT语句? 这样做不是把所有可屏蔽中断都屏蔽掉了?那如何才能响应下一个中断呢?

2. PieCtrlRegs.PIEIER9.all = TempPIEIER; 为什么要执行这一局?要把原先PIEIER9里面的值恢复?为什么这样做?
3. IER |= M_INT9;
IER &= MINT; 这两句我推导过,的确是使 大于第9组中断级别的中断使能,小于第9组中断级别的中断不使能,但是这样之后小于第9组的中断级别的中断的IER使能位已经被写0了,那如何才能执行低级的中断?