This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

中断:高优先级中断被低优先级中断打断疑惑?




 

如题:

设置了两个中断,1>   XINT1_ISR      (INT1.4)

           以及              2>   EPWM1_INT_ISR  (INT3.1)

分别在对应中断处理中,加入IO翻转,测试中断时序。

由于XINT1_ISR中断优先级高,理论上当XINT1_ISR退出中断后,EPWM中断才能触发且对应IO电平拉高,

但是实际上,在XINT1_ISR中断执行期间,EPWM中断也触发了:出现了XITN1_ISR中断挂起,执行EPWM中断的过程,

请问有人知道是啥原因吗?

中断优先级采用默认的

 

// INT 1.4

void  XINT1_ISR(void)
{
   // Insert ISR Code here

 GpioDataRegs.GPBSET.bit.GPIO32 = 1;
 test(); 
 GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1;

   // To receive more interrupts from this PIE group, acknowledge this interrupt
 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}

 

// INT 3.1
void EPWM1_INT_ISR(void)     // EPWM-1
{
       GpioDataRegs.GPASET.bit.GPIO27 = 1;//
       TEST1();
       GpioDataRegs.GPACLEAR.bit.GPIO27 = 1;//
       // Clear INT flag for this timer
       EPwm1Regs.ETCLR.bit.INT = 1;
       // To receive more interrupts from this PIE group, acknowledge this interrupt
       PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}