This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

更换烧毁的28335后,SRAM ZONE7 data verification error



大家好!

LZ不才,烧了两块28335核心,于是买来芯片换上,两片开发板是一样的,LZ用到了SRAM(IS61LV51216),映射在ZONE7.

第一块板子修复成功,另一块不走运,下载程序时报错: load program error ...... a data verification error occurred,  file load failed.(所用工程文件与第一块板子一模一样)

但是我下载不使用SRAM的程序进去,就能正常运行,初步分析是SRAM问题。

检查管脚连接和供电,都正常,对于硬件检查大家有什么建议呢?

看到www.deyisupport.com/.../66439.aspx

说可以在下载程序之前连接DSP看memory,LZ死活没找到方法,也请大家示教,CCS6.0  XDS100V3

  • 补充一下,看help manual,有这样的描述,可是lz居然找不到这个button

    Connect/Disconnect functioanlity is applicable to hardware targets only.

    Note: When the Debug Project command performs, the hardware target is automatically connected.

    Launching debugger from target configurations view does not automtically connect to the target. Connection to the target can be established by clicking on  connect button.

  • DEBUG时会自动连接        我一直是这样使用的   

    你问题中的按钮没看到是什么图图       

    但是你前面的问题    与连接没关系啊      下载的时候只是与外扩存储有关系还是与

    整个工程的大小有关系啊       你看看GEL文件有没有问题