我记得以前好像看到过官网上说F28M35通过了IEC61508,但是现在又找不到了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
F28M35没有过这个标准的,TI的安全芯片是Hercules, 通过了61508、62262等,建议在safety网页上寻找:
http://www.ti.com/ww/en/functional_safety/safeti/SafeTI-61508.html
最近在用TI的Concerto系列F28M35H52C 做一个模拟信号采集的项目。在ADC方面遇到一些问题。不知是否方便予以解答。前两天在deyisupport上发过帖子,但没人回答,故现在想你求援。
问题描述:在我的设计中,ADC1/ADC2采用overlap、依次顺序进行转换,各SOC0--SOC15均采用定时器TINT1的100us定时去触发,当SOC15转换完毕后去触发ADCINT1(ADC2的SOC15触发ADCINT2),ADCINT1/ADCINT2在PIE中不允许中断,通过查询中断标记位判断16个SOC转换是否完成。在程序中在各步加设GIO置1或0的方式,通过示波器观察各步的执行时间和状态,发现采用查询ADCINT1中断标记位时,从ADC启动(通过TINT1启动)到ADC1 的中断标记置位时的时间间隔只有惊人的0.8us这么短,那可是16个SOC的转换啊!根据TI的SPRUH22F中P900到的参数,应该是543ns X 16=8.5us左右,差距是10倍左右!而采用查询ADCCTL1.bit.ADCBSY和ADCCTL1.bit.ADCBSYCHN方式,测得到SOC15转换完毕的时间大约8us,还算靠谱! 通过设置断点,发现在中断标记为置位时,ADCBSY=1,且ADCBSYCHN=2,说明在SOC1转换完毕时,就触发了中断!但在初始化代码中,明明是设置的SOC15。
Adc1Regs.INTSEL1N2.bit.INT1SEL = 15; // setup ADC1 EOC15 to trigger ADCINT1
不知是什么原因。
我的问题就是:如何通过查询相关的ADCINT1中断标记位,判断16个SOC转换是否完成?
ADCINT1/ADCINT2和TINT1均允许中断,但在PIE中却不允许中断,通过查询方式进行判断。
以下是相关的程序代码,请帮忙看看是否有问题!谢谢!
由于自己设计的硬件还在打样中。所以目前硬件用的还是Concerto F28M35xx controlCARD。软件是在\ti\controlSUITE\device_support\f28m36x\v206修改的。
EALLOW;
Adc1Regs.ADCCTL1.bit.ADCBGPWD = 1; // Power ADC1 BG, Bandgap circuit(带隙基准电路) 上电, 见TRM P911 ADCCTL1
Adc1Regs.ADCCTL1.bit.ADCREFPWD = 1; // Power reference,Reference buffers circuit power down
Adc1Regs.ADCCTL1.bit.ADCPWDN = 1; // Power ADC1, ADC power down
Adc1Regs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC1
Adc1Regs.ADCCTL1.bit.ADCREFSEL = 0; // Select interal BG, Internal/external reference select
Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 0; // 0--Enable overlap mode
Adc1Regs.ADCCTL1.bit.INTPULSEPOS = 1; // ADCINT1 trips after AdcResults latch
Adc1Regs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
Adc1Regs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
Adc1Regs.INTSEL1N2.bit.INT1SEL = 15; // setup ADC1 EOC15 to trigger ADCINT1
Adc1Regs.SOCPRICTL.bit.SOCPRIORITY = 15; // 15: SOC0-SOC14 are high priority, SOC15 is in round robin mode.
AnalogSysctrlRegs.TRIG1SEL.all = 2; // Assigning TINT1 (CPU Timer 1) to ADC TRIGGER 1 of the ADC1 and ADC2 module
Adc1Regs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADC1A0
Adc1Regs.ADCSOC1CTL.bit.CHSEL = 8; // set SOC1 channel select to ADC1B0
Adc1Regs.ADCSOC2CTL.bit.CHSEL = 4; // set SOC2 channel select to ADC1A4
Adc1Regs.ADCSOC3CTL.bit.CHSEL = 12; // set SOC3 channel select to ADC1B4
Adc1Regs.ADCSOC4CTL.bit.CHSEL = 0; // set SOC4 channel select to ADC1A0
Adc1Regs.ADCSOC5CTL.bit.CHSEL = 8; // set SOC5 channel select to ADC1B0
Adc1Regs.ADCSOC6CTL.bit.CHSEL = 4; // set SOC6 channel select to ADC1A4
Adc1Regs.ADCSOC7CTL.bit.CHSEL = 12; // set SOC7 channel select to ADC1B4
Adc1Regs.ADCSOC8CTL.bit.CHSEL = 0; // set SOC8 channel select to ADC1A0
Adc1Regs.ADCSOC9CTL.bit.CHSEL = 8; // set SOC9 channel select to ADC1B0
Adc1Regs.ADCSOC10CTL.bit.CHSEL = 4; // set SOC10 channel select to ADC1A4
Adc1Regs.ADCSOC11CTL.bit.CHSEL = 12; // set SOC11 channel select to ADC1B4
Adc1Regs.ADCSOC12CTL.bit.CHSEL = 0; // set SOC12 channel select to ADC1A0
Adc1Regs.ADCSOC13CTL.bit.CHSEL = 8; // set SOC13 channel select to ADC1B0
Adc1Regs.ADCSOC14CTL.bit.CHSEL = 4; // set SOC14 channel select to ADC1A4
Adc1Regs.ADCSOC15CTL.bit.CHSEL = 12; // set SOC15 channel select to ADC1B4
Adc1Regs.ADCSOC0CTL.bit.TRIGSEL = 5; // Set SOC0 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC1CTL.bit.TRIGSEL = 5; // set SOC1 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC2CTL.bit.TRIGSEL = 5; // Set SOC2 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC3CTL.bit.TRIGSEL = 5; // set SOC3 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC4CTL.bit.TRIGSEL = 5; // Set SOC4 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC5CTL.bit.TRIGSEL = 5; // set SOC5 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC6CTL.bit.TRIGSEL = 5; // Set SOC6 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC7CTL.bit.TRIGSEL = 5; // set SOC7 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC8CTL.bit.TRIGSEL = 5; // Set SOC8 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC9CTL.bit.TRIGSEL = 5; // set SOC9 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC10CTL.bit.TRIGSEL = 5; // Set SOC10 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC11CTL.bit.TRIGSEL = 5; // set SOC11 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC12CTL.bit.TRIGSEL = 5; // Set SOC12 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC13CTL.bit.TRIGSEL = 5; // set SOC13 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC14CTL.bit.TRIGSEL = 5; // Set SOC14 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC15CTL.bit.TRIGSEL = 5; // set SOC15 start trigger to ADC Trigger 1 of the ADC
Adc1Regs.ADCSOC0CTL.bit.ACQPS = 6; // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC1CTL.bit.ACQPS = 6; // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC2CTL.bit.ACQPS = 6; // set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC3CTL.bit.ACQPS = 6; // set SOC3 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC4CTL.bit.ACQPS = 6; // set SOC4 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC5CTL.bit.ACQPS = 6; // set SOC5 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC6CTL.bit.ACQPS = 6; // set SOC6 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC7CTL.bit.ACQPS = 6; // set SOC7 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC8CTL.bit.ACQPS = 6; // set SOC8 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC9CTL.bit.ACQPS = 6; // set SOC9 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC10CTL.bit.ACQPS = 6; // set SOC10 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC11CTL.bit.ACQPS = 6; // set SOC11 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC12CTL.bit.ACQPS = 6; // set SOC12 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC13CTL.bit.ACQPS = 6; // set SOC13 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC14CTL.bit.ACQPS = 6; // set SOC14 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
Adc1Regs.ADCSOC15CTL.bit.ACQPS = 6; // set SOC15 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
EDIS;
while(CpuTimer1Regs.TCR.bit.TIF==0); //This flag gets set when the CPU-timer decrements to zero, 100us
CpuTimer1Regs.TCR.bit.TIF = 1; // Writing a 1 to this bit clears the flag
POINTPULSE_DAT_REG = 1; // GPIO31-- point pulse, point sanmple strat
//while((Adc1Regs.ADCCTL1.bit.ADCBSY !=0) ||(Adc1Regs.ADCCTL1.bit.ADCBSYCHN != 0x0f));
// 判断BUSY是否空闲,且最后一个通道是否是SOC15
while(Adc1Regs.ADCINTFLG.bit.ADCINT1==0); // 等待ADCINT1信号产生(由SOC15转换完毕产生)
Adc1Regs.ADCINTFLGCLR.bit.ADCINT1 = 1; // 清除ADCINT1中断信号
POINTPULSE_DAT_REG = 0; // high level width: 16 socs total time(include: Sample time + Conversion Time)
以上问题,希望解答!谢谢!
按我的理解,F28M35x做IEC61508或SIL3认证的可能性不大!像Safe MCU---TMS570/RM48X系列,内部都是Dual CPUs的1OO1架构,而F28M35x虽然也是双CPU架构,一个DSP核,一个M3核,它们只是协同工作,不具备1OO1架构,所以不满足 最基本的安全架构。如果有安全级别的需求,还是要选TMS570/RM48X系列,它们是通过认证的,在芯片的Datasheet上明确有讲到它是通过SIL3认证的。如果没有提到,那肯定就没有通过认证。
两年前,我们在做一个门控项目时,是选C2000系列,还是选570系列,当时也比较纠结。后来选了570,现在看来,选择是正确的。还是看看TMS570/RM48X系列吧,最近新推了许多芯片,选择多。
FYI !
@一方☆通行 您好!
看帖子知道你在用F28M35做研发,应该是大牛了!我最近也正在用F28M35设计产品,由于没有经验,遇到点问题,进展不顺!不知是否方便给予解答?谢谢!
问题就是:当VREG12EN接GND,即采用内部电压调整器时,在Layout时,F28M35的VDD12电源引脚:Pin11,24,55,58,66,75,90,99之间是否要在芯片外部彼此连在一起?还是各引脚只需各自接去耦电容就可以了?同理当VREG18EN接GND,VDD18的Pin1,108之间呢?
按照以前TI的FAE的说法,这些引脚在芯片外部是可以不接在一起,因为在芯片内部已经接在一起了,只需各自接去耦电容就可以了!是这样吗?您是怎样做得呢?麻烦解答,不甚感谢!
回答也可以发至:leeanfux@sina.com。
Adc1Regs.SOCPRICTL.bit.SOCPRIORITY = 16也试过了,也不行!连运行状态都不对了! Adc1Regs.SOCPRICTL.bit.SOCPRIORITY = 16的意思是:All SOCs are in high priority mode, arbitrated by SOC number!而Adc1Regs.SOCPRICTL.bit.SOCPRIORITY = 0的意思是:SOC priority is handled in round robin mode for all channels。按我的理解:=16 和 =0的意义是一样的,是不是!但运行情况不同!
不是太阳能库,是controlCARDs下面的DIM100硬件啊入门模块,ORCAD打开。另外提供一份开发板的原理图供参考。
@一方☆通行,您好!
谢谢您的解答及原理图!从原理图来看,您用的资源较多,较高端!看来您钻研的深,向您学习!
我的打样的硬件基本能跑了。关于当VREG12EN接GND时,F28M35的VDD12电源引脚:Pin11,24,55,58,66,75,90,99之间在芯片外部不用彼此连在一起!各引脚只需各自接去耦电容就可以了?同理当VREG18EN接GND,VDD18的Pin1,108之间也是一样!这样便于PCB的Layout时。
我看你ADC用的较充分,那关于ADC的SOC转换序列的最后一个SOC15转换完成,您是如何查询的呢?是中断?还是查询?在调试中,通过设置断点,发现在中断标记为置位时,ADCBSY=1,且ADCBSYCHN=2,说明在SOC1转换完毕时,就触发了中断!但在初始化代码中,明明是设置的SOC15。
回答也可以发至:leeanfux@sina.com。不甚感谢!
我曾用570的20216设计过产品,如有需求,可尽力而为!