如果从外部XINTF扩展的flash启动,那么启动加载BOOT选项到底该选哪个?手册上说的有6种:
1:Jump to Flash/ROM address 0x3F 7FF6. 前面说的从内部flash启动选择此方法
2:Call SPI_Boot to load from an external serial SPI EEPROM
3:Call SCI_Boot to load from SCI-A
4:Jump to H0 SARAM address 0x3F 8000
5:Jump to OTP address 0x3D 7800
6:Call Parallel_Boot to load from GPIO Port B
那么从XINTF启动,在以上6种模式中,靠边儿的只有第一种了,那么是不是说,从外部XINTF接口闪存启动,还是要在内部闪存0x3F 7FF6位置实现写入跳转指令呢?