This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

自制28335控制板3.3V不稳造成程序跑飞?



大家好!

LZ照着购置的28335开发板的原理图设计了一块控制板。最小系统中,除了电源模块不同(开发板是5V->3.3V,自制是32->3.3V LM2675LD-3.3),其他都一样。3.3V还带了很多外围器件,但总体功率都计算过。

在开发板上正常运行的RAM程序,直接烧录至自制板上,运行时会出现进各种中断的情况(illegal_isr、XXX_isr)或者JTAG报错(low power mode等等等)。

裁剪程序至只有系统主频设定150MHz和主循环中加delay_us,发现程序运行仍旧时好时坏,但通过肉眼观察3.3V电源指示LED(后经示波器验证),发现程序异常时3.3V有一瞬间被拉低至不足3V(多数出现在点击运行程序时,也有程序运行中),之后程序必定异常。而购置开发板点击运行程序和运行中不会出现这样的情况。

请问大家这个3.3V异常是否就是导致我程序异常的原因,还是有别的?3.3V故障该按什么思路去排除呢?(静态测量下DSP 3.3V、1.9V供电都正常)

谢谢!