This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069的cmd



请问谁那里有28069的Flash和cla的cmd文件,请给发一份

  • 和RAM_CLA的CMD文件差不多,只是代码下载到flash地址不一样,还有CLA的代码放的地址。可以在RAM_CLA的基础上改下。

  • 以下可以供你参考,主要加了CLA的DATA MEMEORY和rogram memory,这个CMD是用于数字电源的应用,加入了TI 数字电源库的东西。直接复制黏贴到你的原来CMD就可以

    /*
    //###########################################################################
    //
    // FILE: F28069_CLA.cmd
    //
    // TITLE: Linker Command File For F28069 Device
    //
    //###########################################################################
    // $TI Release: F2806x C/C++ Header Files and Peripheral Examples V136 $
    // $Release Date: Apr 15, 2013 $
    //###########################################################################
    */

    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\F2806x_headers\cmd
    //
    // For BIOS applications add: F2806x_Headers_BIOS.cmd
    // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd
    ========================================================= */

    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map */

    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l F2806x_Headers_nonBIOS.cmd */

    /* Uncomment this line to include file only for BIOS applications */
    /* -l F2806x_Headers_BIOS.cmd */

    /* 2) In your project add the path to <base>\F2806x_headers\cmd to the
    library search path under project->build options, linker tab,
    library search path (-i).
    /*========================================================= */

    /* Define the memory block start/length for the F2806x
    PAGE 0 will be used to organize program sections
    PAGE 1 will be used to organize data sections

    Notes:
    Memory blocks on F28069 are uniform (ie same
    physical memory) in both PAGE 0 and PAGE 1.
    That is the same memory region should not be
    defined for both PAGE 0 and PAGE 1.
    Doing so will result in corruption of program
    and/or data.

    Contiguous SARAM memory blocks can be combined
    if required to create a larger memory block.
    */
    CLA_SCRATCHPAD_SIZE=0x30;
    _Cla1Prog_Start = _Cla1funcsRunStart;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start


    MEMORY
    {
    PAGE 0 : /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    CLAProg : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    C28Prog : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
    FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
    FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
    FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
    FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
    FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
    FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
    FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
    IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    CLARAM0 : origin = 0x008800, length = 0x000400 /* CLA RAM0 2K */
    CLARAM1 : origin = 0x008C00, length = 0x000400 /* CLA RAM1 1K */
    CLARAM2 : origin = 0x008000, length = 0x000800 /* CLA RAM2 1K */
    dataRam : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */
    RAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */
    RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */
    RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */
    USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */
    FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */

    CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA to CPU RAM */
    CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU to CLA RAM */

    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */


    SECTIONS
    {

    /* Allocate program areas: */
    .cinit : > FLASHA, PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : > FLASHA, PAGE = 0
    codestart : > BEGIN, PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = C28Prog,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    PAGE = 0
    {
    --library=Solar_Lib_Float.lib<CNTL_2P2Z_F_ASM.obj>
    --library=Solar_Lib_Float.lib<CNTL_3P3Z_F_ASM.obj>
    }


    Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */
    RUN = CLAProg,
    LOAD_START(_Cla1funcsLoadStart),
    LOAD_END(_Cla1funcsLoadEnd),
    RUN_START(_Cla1funcsRunStart),
    PAGE = 0

    csmpasswds : > CSM_PWL_P0, PAGE = 0
    csm_rsvd : > CSM_RSVD, PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM0, PAGE = 1
    .ebss : > dataRam, PAGE = 1
    .esysmem : > RAMM1, PAGE = 1

    /* Initalized sections to go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHA, PAGE = 0
    .switch : > FLASHA, PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : LOAD = FLASHA,
    RUN = C28Prog,
    LOAD_START(_IQfuncsLoadStart),
    LOAD_END(_IQfuncsLoadEnd),
    RUN_START(_IQfuncsRunStart),
    PAGE = 0

    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    /* Allocate FPU math areas: */
    FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS, PAGE = 0, TYPE = DSECT

    cntl_coeff_RAM : > dataRam, PAGE=1
    cntl_var_RAM : > dataRam, PAGE =1

    Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
    CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1

    ClaDataRam0 : > CLARAM0, PAGE = 1
    ClaDataRam1 : > CLARAM1, PAGE = 1
    ClaDataRam2 : > CLARAM2, PAGE = 1
    CLAmathTables : > CLARAM1, PAGE = 1
    CLA1mathTables : > CLARAM1, PAGE = 1

    CLAscratch :
    { *.obj(CLAscratch)
    . += CLA_SCRATCHPAD_SIZE;
    *.obj(CLAscratch_end) } > CLARAM0, PAGE = 1

    /* Uncomment the section below if calling the IQNexp() or IQexp()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

    }
    */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

    /* .reset is a standard section used by the compiler. It contains the */
    /* the address of the start of _c_int00 for C Code. /*
    /* When using the boot ROM this section and the CPU vector */
    /* table is not needed. Thus the default type is set here to */
    /* DSECT */


    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */