This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: 外部晶振驱动在运行过程中停止工作

Part Number: TMS320F280049


您好,

       我们在一款充电机产品的高温测试时遇到一个问题,系统运行一段时间后,F280049的CAN报文停发,且无法恢复。检查后发现芯片的外部晶振输入引脚X1电平保持为低电平,晶振未工作,XRSn引脚电平每隔16.8ms拉低一次再拉高。更换F280049芯片后系统恢复正常;

       外部供电3.3V,VDD 1.2V均稳定无波动,我们无法定位芯片的晶振输入引脚损坏的原因,请帮忙分析,多谢!