This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: xds100v3正常换xds200仿真器连不上芯片

Part Number: TMS320F280049


xds100v3用了很多年,最近因嫌仿真效率低,买了xds200,连不上目标芯片。

现象:

1. 同事电脑拿过来,把xds200仿真器连到他电脑上,ccs连通测试正常,说明硬件&仿真器&线缆都没问题,问题出在我电脑上。

2. CCS版本:12.5.0.00007, 重装过也不行; win11系统,设备管理器可识别到xds2xx,如下图

   

3. 测试log

[Start: Texas Instruments XDS2xx USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\fansh\AppData\Local\TEXASI~1\CCS\
ccs1250\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Sep 6 2023'.
The library build time was '14:47:53'.
The library package version is '9.13.0.00201'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

This emulator does not create a reset log-file.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-230' (0xffffff1a).
The title is 'SC_ERR_PATH_MEASURE'.

The explanation is:
The measured lengths of the JTAG IR and DR scan-paths are invalid.
This indicates that an error exists in the link-delay or scan-path.

[End: Texas Instruments XDS2xx USB Debug Probe_0]