您好:
我看到dsp2808的PLL可以选择倍频10倍,那我晶振输入为20M的话,主频岂不是变为200M了?但是又说2808的主频是100M,这个怎么理解啊?倍频和晶振频率之间的关系是不是有限制?谢谢!
另外使用28335的话,一定要用ccs4.0版本吗?谢谢!
祝好!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我看到dsp2808的PLL可以选择倍频10倍,那我晶振输入为20M的话,主频岂不是变为200M了?但是又说2808的主频是100M,这个怎么理解啊?倍频和晶振频率之间的关系是不是有限制?谢谢!
另外使用28335的话,一定要用ccs4.0版本吗?谢谢!
祝好!
200M还要分频啊,分频成100M,有乘法还要有除法。
100M是最高的主频。
28335可以用CCS3.3,CCS4.2,CCS5.1等,CCS3.3对F28335支持的。
请问28335用CC3.3与用CCS4.0有什么区别?在control里面没看到有ccs3.3的例子,是ccs4.0的,这样就打不开了
以后TI都会用CCS4以上版本。
区别就是CCS4以上版本是基于Elipcs平台的。
Control Suite上的历程也是基于CCSv4或者v5的。
那用ccs3.3来编译28335的程序,执行时间会与用ccs4.0编译有差别吗,也就是C反汇编的效率有没有不同
编译器相同,所以效率就相同。
换句话说,您可以自己用DOS语言来调用编译器对程序进行编译,效率是和CCS无关的。