Other Parts Discussed in Thread: PCF8574
现在在f28335上用PCF8574扩展IO口,上拉电阻也弄了,ID也反复检查了,但还是调试不通,很着急,希望大家能指导一下,谢谢了,下面是我的代码,大家看一下,是不是哪里配置不正确(另:这段代码运行一次后,在运行第二次、第三次......那个总是提示总线繁忙I2caRegs.I2CSTR.bit.BB 这个位总是1):
#define I2C_SLAVE_ADDR 0x40
void I2CA_Init(void)
{
I2caRegs.I2CSAR = 0x0040; // Slave address - EEPROM control code
#if (CPU_FRQ_150MHZ) // Default - For 150MHz SYSCLKOUT
I2caRegs.I2CPSC.all = 14; // Prescaler - need 7-12 Mhz on module clk (150/15 = 10MHz)
#endif
#if (CPU_FRQ_100MHZ) // For 100 MHz SYSCLKOUT
I2caRegs.I2CPSC.all = 9; // Prescaler - need 7-12 Mhz on module clk (100/10 = 10MHz)
#endif
I2caRegs.I2CCLKL = 10; // NOTE: must be non zero 时钟总线SCL低电平持续时间
I2caRegs.I2CCLKH = 5; // NOTE: must be non zero 时钟总线SCL高电平持续时间
I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY interrupts
I2caRegs.I2CMDR.all = 0x0020; // Take I2C out of reset
// Stop I2C when suspended
I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO
I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT,
return;
}
Uint16 I2cWriteRegister(Uint16 i2cAddr,Uint16 data1,Uint16 data2)
{
if (I2caRegs.I2CMDR.bit.STP == 1) //停止条件控制位
{
return I2C_STP_NOT_READY_ERROR;
}
I2caRegs.I2CSAR = i2cAddr;
if (I2caRegs.I2CSTR.bit.BB == 1) //BB =1 总线繁忙,BB = 0 总线空闲
{
return I2C_BUS_BUSY_ERROR;
}
I2caRegs.I2CCNT = 2;
// Setup data to send
I2caRegs.I2CDXR = data1;
I2caRegs.I2CDXR = data2;
// Send start as master transmitter
I2caRegs.I2CMDR.all = 0x6E20;
DSP28x_usDelay(100000);
return I2C_SUCCESS;
}
void Write_PCF8574(Uint16 data1,Uint16 data2)
{
I2cWriteRegister(0x40,data1,data2);
}
void I2C_Pcf()
{
InitI2CGpio();
I2CA_Init();
while(1)
{
Write_PCF8574(0x00,0x00);
DSP28x_usDelay(2000000);
}
}