This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: 库函数使用

Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE

我尝试在280039芯片的boot中使用CMAC校验application 来完成安全启动。

首先,我将C:\ti\c2000\C2000Ware_5_03_00_00\libraries\boot_rom\f28003x\rev0\rom_symbol_libs\secureZone中的“F28003x_SecureZoneCodeSymbols_fpu32.lib”文件复制到我的工程中;

然后,按照C:\ti\c2000\C2000Ware_5_03_00_00\driverlib\f28p65x\examples\c28x\boot中的示例那样在.c文件中使用CPU1BROM_calculateCMAC()函数;

但编译的时候出现警告:#10373-D F28003x_SecureZoneCodeSymbols_fpu32.lib" contains ELF object files which are incompatible with the TI-COFF output file. 

同时出现错误#10234-D: unresolved symbols remain。

可以提供 F28003x_SecureZoneCodeSymbols_fpu32.lib 为 legacy COFF格式的库文件吗?

因为将工程更改output format格式的话,工作量较大。