This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dap的ad采样



您好:

  ad采样有顺序采样和同时采样两种方式,如果我要采集8路信号,可以采用顺序采样,也可以采用同时采样,那么这两种采样方式对程序执行时间有区别没有?也就是说用哪种方式会更快点?

另外ad转换时钟的问题,是不是设置的时钟越高,采样速度就越快,但是会不准确?一般24X系列的设置为多少?谢谢!

  • 1. 同时采样,顾名思义,可以两路信号同时采样保持,先后转换。 当你有相位一致或者同步采样的要求时,建议用同步采样。例如必须同时采样一路电流和电压信号。程序执行时间相差无几,因为是同一个AD核心,即使同时采样,也要分别转换。

    2. 采样频率是从AD时钟分频来的,所以有一点关系,但无绝对关系。采样频率和信号有关,至少是信号的2.56倍。越高当然越精细,但对CPU的主频要求较高。低于2倍,就不符合采样定律了。