This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c2407程序跑飞



c2000系列DSP2407程序跑飞现象描述:
供电:由12v经LM7805先转换成5v,经过TPS7333产生3.3v;
复位:DSP设置硬件复位,由max811产生;同时软件有看门狗;
过程:上电后工作正常,2秒钟后12v电源有较大负载产生电压跌落,进而影响5v和3.3v电压,示波器观测到较大电压干扰,系统有时会复位,但有时会跑飞,进入不确定状态。
问题:怎么能保证系统在电源异常时可以复位,不导致系统跑飞?系统设置了硬件复位和看门狗,为什么还会跑飞?

  • 经过多番实验,发现跑飞的原因为空间电磁干扰导致,另一个电路板的开关电源产生噪声,干扰到DSP正常运行,将电路板垫高,距离干扰源远点,问题解决。

    起初一直怀疑电源问题,今天把电源加入共模电感,已经很干净,DSP仍然会跑飞。