本人用tms320F28035做永磁同步电机控制,将Epwm1/2/3配置成互补的PWM输出,时钟同步上将ePWM1为主pwm,epwm2/3为从pwm。实验时出现奇怪的现象:有时候上电后,epwm1/2/3都能正常输出;有时候上电后,epwm1能够正常输出,epwm2/3没有输出(都是直接测量的DSP管脚)。请问,这可能是什么原因?
PWM配置代码如下:
//-------------------------------------------------------------
//初始化Epwm1的寄存器
//-------------------------------------------------------------
void InitEPwm1(void)
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
// Setup TBCLK
EPwm1Regs.TBPRD = 3000; // Set timer period 801 TBCLKs
EPwm1Regs.TBCTR = 0x0000; // Clear counter
EPwm1Regs.TBCTL.bit.PHSDIR = 0;
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
// Set Compare values
EPwm1Regs.CMPA.half.CMPA = 1500; // Set compare A Init value
EPwm1Regs.CMPB = 1500; // Set Compare B Init value
// Setup counter mode
EPwm1Regs.TBCTL.bit.CTRMODE = 0x2; // Up-dowm Counter mode
EPwm1Regs.TBCTL.bit.PHSEN = 0; // Master Module
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x0; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = 0x0; //60MHZ/(1*1) = 60MHZ,EPWM模块始终频率为60MHZ
EPwm1Regs.TBCTL.bit.PRDLD = 0;
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1;
// Setup shadowing
EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0x0;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0x0;
EPwm1Regs.CMPCTL.bit.LOADAMODE = 0x0; // Load on Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = 0x0;
// Set actions
EPwm1Regs.AQCTLA.bit.CAU = 0x2; // Set PWM1A High on event A, up count
EPwm1Regs.AQCTLA.bit.CAD = 0x1; // Clear PWM1A Low on event A, down count
EPwm1Regs.AQCTLB.bit.CBU = 0x1;
EPwm1Regs.AQCTLB.bit.CBD = 0x2;
// ENABLE TRIG ADC
EPwm1Regs.ETSEL.bit.SOCAEN = 1; //
EPwm1Regs.ETSEL.bit.SOCASEL = 1; //
EPwm1Regs.ETPS.bit.SOCAPRD = 1;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
}
//-------------------------------------------------------------
//初始化Epwm2的寄存器
//-------------------------------------------------------------
void InitEPwm2(void)
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // DISEnable TBCLK within the ePWM
EDIS;
// Setup TBCLK
EPwm2Regs.TBPRD = 3000; // Set timer period 801 TBCLKs
EPwm2Regs.TBCTR = 0x0000; // Clear counter
EPwm2Regs.TBCTL.bit.PHSDIR = 1;
EPwm2Regs.TBPHS.half.TBPHS = 0x0002; // Phase is 2
// Set Compare values
EPwm2Regs.CMPA.half.CMPA = 1500; // Set compare A Init value
EPwm2Regs.CMPB = 1500; // Set Compare B Init value
// Setup counter mode
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // Up-dowm Counter mode
EPwm2Regs.TBCTL.bit.PHSEN = 1; // Slave Module
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = 0; //60MHZ/(1*1) = 60MHZ,EPWM模块始终频率为60MHZ
EPwm2Regs.TBCTL.bit.PRDLD = 0;
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0;
// Setup shadowing
EPwm2Regs.CMPCTL.bit.SHDWAMODE = 0;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm2Regs.CMPCTL.bit.LOADAMODE = 0; // Load on Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = 0;
// Set actions
EPwm2Regs.AQCTLA.bit.CAU = 2; // Set PWM2A High on event A, up count
EPwm2Regs.AQCTLA.bit.CAD = 1; // Clear PWM2A Low on event A, down count
EPwm2Regs.AQCTLB.bit.CBU = 1;
EPwm2Regs.AQCTLB.bit.CBD = 2;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // DISEnable TBCLK within the ePWM
EDIS;
}
//-------------------------------------------------------------
//初始化Epwm3的寄存器
//-------------------------------------------------------------
void InitEPwm3(void)
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // DISEnable TBCLK within the ePWM
EDIS;
// Setup TBCLK
EPwm3Regs.TBPRD = 3000; // Set timer period 801 TBCLKs
EPwm3Regs.TBCTR = 0x0000; // Clear counter
EPwm3Regs.TBCTL.bit.PHSDIR = 1;
EPwm3Regs.TBPHS.half.TBPHS = 0x0002; // Phase is 2
// Set Compare values
EPwm3Regs.CMPA.half.CMPA = 1500; // Set compare A Init value
EPwm3Regs.CMPB = 1500; // Set Compare B Init value
// Setup counter mode
EPwm3Regs.TBCTL.bit.CTRMODE = 2; // Up-dowm Counter mode
EPwm3Regs.TBCTL.bit.PHSEN = 1; // Slave Module
EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = 0; //60MHZ/(1*1) = 60MHZ,EPWM模块始终频率为60MHZ
EPwm3Regs.TBCTL.bit.PRDLD = 0;
EPwm3Regs.TBCTL.bit.SYNCOSEL = 0;
// Setup shadowing
EPwm3Regs.CMPCTL.bit.SHDWAMODE = 0;
EPwm3Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm3Regs.CMPCTL.bit.LOADAMODE = 0; // Load on Zero
EPwm3Regs.CMPCTL.bit.LOADBMODE = 0;
// Set actions
EPwm3Regs.AQCTLA.bit.CAU = 2; // Set PWM3A High on event A, up count
EPwm3Regs.AQCTLA.bit.CAD = 1; // Clear PWM3A Low on event A, down coun
EPwm3Regs.AQCTLB.bit.CBU = 1;
EPwm3Regs.AQCTLB.bit.CBD = 2;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // DISEnable TBCLK within the ePWM
EDIS;
}
//-------------------------------------------------------------
//初始化Epwm1中TripZone的寄存器
//-------------------------------------------------------------
void InitTripZone(void)
{
EALLOW;
EPwm1Regs.TZSEL.bit.OSHT1 = 1;
EPwm2Regs.TZSEL.bit.OSHT1 = 1;
EPwm3Regs.TZSEL.bit.OSHT1 = 1;
EPwm1Regs.TZCTL.bit.TZA = 2; //Pull down EPWM1A When oneshot Trip Event Occure
EPwm1Regs.TZCTL.bit.TZB = 2; //Pull down EPWM1B When oneshot Trip Event Occure
EPwm2Regs.TZCTL.bit.TZA = 2; //Pull down EPWM2A When oneshot Trip Event Occure
EPwm2Regs.TZCTL.bit.TZB = 2; //Pull down EPWM2B When oneshot Trip Event Occure
EPwm3Regs.TZCTL.bit.TZA = 2; //Pull down EPWM3A When oneshot Trip Event Occure
EPwm3Regs.TZCTL.bit.TZB = 2; //Pull down EPWM3B When oneshot Trip Event Occure
EPwm1Regs.TZEINT.bit.OST = 1; //Enable interrupt EPWM1_TZINT
EDIS;
}