您好,我建立了一个工程文件,利用28335.cmd文件编译没有问题,但改为28335_RAM_lnk.cmd文件后,就报错,具体如下:
不知道是怎么回事?请您多多指教。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我建立了一个工程文件,利用28335.cmd文件编译没有问题,但改为28335_RAM_lnk.cmd文件后,就报错,具体如下:
不知道是怎么回事?请您多多指教。谢谢!
您好,具体内容为:
undefined first referenced symbol in file --------- ---------------- _RamfuncsLoadEnd C:\\Users\\whx\\Desktop\\CPU_DSP_100503\\CPU_DSP_100503\\AD6K_S_QGX_Pro\\sys\\build\\Debug\\28335_TR.obj _RamfuncsLoadStart C:\\Users\\whx\\Desktop\\CPU_DSP_100503\\CPU_DSP_100503\\AD6K_S_QGX_Pro\\sys\\build\\Debug\\28335_TR.obj _RamfuncsRunStart C:\\Users\\whx\\Desktop\\CPU_DSP_100503\\CPU_DSP_100503\\AD6K_S_QGX_Pro\\sys\\build\\Debug\\28335_TR.obj
error: unresolved symbols remain warning: entry-point symbol other than "_c_int00" specified: "code_start" error: errors encountered during linking; "./Debug/Example_2833xCpuTimer.out" not built
>> Compilation failure
Build Complete, 1 Errors, 1 Warnings, 0 Remarks.
然后我就在.c文件中查看了一下上述三个的变量,看到上面有如下定义:
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
然后我又查了一下,在DSP2833x_GlobalPrototypes.h文件中也有一模一样的定义。然后我把.c的定义中的三个extern去掉,如下:
Uint16 RamfuncsLoadStart;
Uint16 RamfuncsLoadEnd;
Uint16 RamfuncsRunStart;,编译通过了。
以上都是选择ram_lnk.cmd文件时出现的情况。然后我打开看了一下28335.cmd文件。看到里面有如下三个变量:
LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart),
我有些搞不懂他们的关系了。
谢谢您!
您好,
是的,如下:
// Step 4. Initialize the Device Peripheral. This function can be /*****************************************************************************************/ MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); InitFlash();
那么,往flash里下载与往ram里下载,不同的就是cmd文件和这个函数吗,是吗?
谢谢!
哦,是这样啊,那就把这个函数屏蔽就行吧,往flash里下载也不用它是吧,谢谢您!