This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: 关于上电时序及上电期间各端口电压要求

Part Number: TMS320F280049

1,我们在实际开发中遇到了芯片损坏问题:大概现象是:反复上下电十几次后出现ADC采样数据异常的问题,已经排除外围电路影响(在不贴装0049的情况下各AD信号电压都正常,贴装之后出现波动、漂高等现象),据此怀疑可能是供电回路或者上电时序存在问题导致0049芯片损坏;

2,在280049的datasheet中,7.9.1.4.2 Signal Pins Power Sequence章节:  Before powering the device,  no voltage larger than 0.3 V above VDDIO or 0.3 V below VSS should be applied to any digital pin... 此处的VDDIO指的是3.3V(假设我设计中的供电电压就是3.3V),还是该描述的上电过程中某一时刻的实际VDDIO电压?   -------------比如在上电过程中的某一时刻,VDDIO 和VDDA 电压才达到1.0V,但某个GPIO和ADC采样输入端口电压是3.3V,会导致7.9.1.4.2 章节中描述的损坏么?