Can you help me to see what is wrong with the Action Qualifier part of the code? Run it and say that it can not open the file.
//#############################################################################
//
// FILE: epwm_ex1_trip_zone.c
//
// TITLE: ePWM Using Trip-Zone Submodule.
//
//! \addtogroup driver_example_list
//! <h1>ePWM Trip Zone</h1>
//!
//! This example configures ePWM1 and ePWM2 as follows
//! - ePWM1 has TZ1 as one shot trip source
//! - ePWM2 has TZ1 as cycle by cycle trip source
//!
//! Initially tie TZ1 high. During the test, monitor ePWM1 or ePWM2
//! outputs on a scope. Pull TZ1 low to see the effect.
//!
//! \b External \b Connections \n
//! - ePWM1A is on GPIO0
//! - ePWM2A is on GPIO2
//! - TZ1 is on GPIO12
//!
//! This example also makes use of the Input X-BAR. GPIO12 (the external
//! trigger) is routed to the input X-BAR, from which it is routed to TZ1.
//!
//! The TZ-Event is defined such that ePWM1A will undergo a One-Shot Trip
//! and ePWM2A will undergo a Cycle-By-Cycle Trip.
//!
// _____________ __________________
// | | | |
// GPIO12 -----| I/P X-BAR |-----TZ1-----| ePWM TZ Module |-----TZ-Event
// |___________| |________________|
//
//
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"
#include <math.h>
//
// Globals
//
//void initEPWM(uint32_t base);
//void updateCompare(epwmInformation *epwmInfo);
//static uint32_t epwm1TZIntCount;
//static uint32_t epwm1IntCount;
//static uint32_t epwm3IntCount;
//
// Function Prototypes
//
uint32_t EPwm1TimerIntCount=0;
__interrupt void epwm1ISR(void);
//__interrupt void epwm1TZISR(void);
uint32_t ISRcount =0;
uint32_t REFA_H =0;
uint32_t REFB_H= 0;
uint32_t REFC_H=0;
uint32_t PhaseShift1=0;
uint32_t PhaseShift2=0;
uint32_t PhaseShift3=0;
uint32_t PhaseShift=0;
uint32_t theta, del_theta;
uint32_t Freq=100,Vm= 5000;
void main(void)
{
Interrupt_initModule();
Interrupt_initVectorTable();
Device_init();
Device_initGPIO();
Interrupt_register(INT_EPWM1, &epwm1ISR);
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
Board_init();
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
Interrupt_enable(INT_EPWM1);
EINT;
ERTM;
EPwm1TimerIntCount++;
while(1)
{
NOP;
}
}
__interrupt void epwm1ISR(void)
{
ISRcount++;
if( ISRcount <=100)
{
GPIO_writePin(myGPIO0, 1); // GPIO58 is high
EPWM_setDeadBandDelayPolarity(myEPWM4_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_HIGH);
EPWM_setCounterCompareValue(myEPWM4_BASE, EPWM_COUNTER_COMPARE_A, 0);
EPWM_setActionQualifierAction(myEPWM4_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM4_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A, 2500);
//EPWM_setCounterCompareValue(myEPWM22_BASE, EPWM_COUNTER_COMPARE_B, 250);
EPWM_setDeadBandDelayPolarity(myEPWM3_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);
EPWM_setDeadBandDelayMode(myEPWM3_BASE, EPWM_DB_RED, true);
EPWM_setRisingEdgeDelayCount(myEPWM3_BASE, 5);
EPWM_setDeadBandDelayMode(myEPWM3_BASE, EPWM_DB_FED, true);
EPWM_setFallingEdgeDelayCount(myEPWM3_BASE, 5);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
}
else if(ISRcount > 100 && ISRcount<=200)
{
GPIO_writePin(myGPIO0, 0); // GPIO58 is high
EPWM_setCounterCompareValue(myEPWM4_BASE, EPWM_COUNTER_COMPARE_A, 0);
EPWM_setActionQualifierAction(myEPWM4_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM4_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWMsettings for S5 and S7
EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A, 2500);
EPWM_setDeadBandDelayPolarity(myEPWM3_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW);
EPWM_setDeadBandDelayMode(myEPWM3_BASE, EPWM_DB_RED, true);
EPWM_setRisingEdgeDelayCount(myEPWM3_BASE, 5);
EPWM_setDeadBandDelayMode(myEPWM3_BASE, EPWM_DB_FED, true);
EPWM_setFallingEdgeDelayCount(myEPWM3_BASE, 5);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
}
else if(ISRcount > 200 && ISRcount<=300)
{ GPIO_writePin(myGPIO0, 1);
}
else if(ISRcount > 300 &&ISRcount<=400)
{ GPIO_writePin(myGPIO0, 0);
}
else
{
ISRcount = 0;
}
EPwm1TimerIntCount++;
GPIO_togglePin(myGPIO11);
PhaseShift=((0xFFFF)*Freq*2*500*0.0000001);
PhaseShift1=PhaseShift1+PhaseShift;
PhaseShift2=(int16_t)Vm*sin((float)PhaseShift1*(0.000095875));
PhaseShift3=fabs(PhaseShift2);
3Info,REFC_H,EPWM1_TIMER_TBPHS);
EPWM_setPhaseShift(myEPWM2_BASE,PhaseShift3);
EPWM_setPhaseShift(myEPWM3_BASE, (PhaseShift3/2));
EPWM_setPhaseShift(myEPWM4_BASE, (PhaseShift3/2));
EPWM_clearEventTriggerInterruptFlag(myEPWM1_BASE);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}