This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
自己做的2812的板子,使用100v1 的仿真器和ccs4.0,我打开集成开发环境然后连接,就出现以下的问题
error connecting to the target:
error 0x80000200/-1142
fata error during:ocs,
processor blocked debug accesses
使用相同的软件配置连接其它的板子,能连上,用自己的板子不能用(所以可以判断仿真器没坏,软件设置正常的),测量了上电后JTAG口的初始电平--与正常板子的一样;再测量芯片的供电----也是正常的;测量RESET脚----有问题的板子RESET脚有2.2--3.3V的文波,正常的板子没有;
请教这样的问题怎么定位,是芯片坏了还是硬件电路搭建有问题,
哪位高手指点指点方向啊,感激不尽