This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812上电引导过程



2812有两种运行模式,微处理器(Microprocessor)模式和微计算机(Microcomputer)模式,复位时,芯片判断XMP/MC引脚上的电平,当该引脚为高电平时,芯片进入微处理器模式,当为低电平时则进入微计算机模式。在微处理器模式下,芯片需要从第7外部接口区引导运行(XINTF Zone 7)。只有在微计算机模式下,芯片才会从内部Boot Rom引导。XMP/MC引脚的状态在复位时锁存入芯片配置寄存器XINTCNF2中MP/MC位,复位后,XMP/MC引脚上的电平就不再有效,芯片将不再关心其状态。用户可以通过改变XINTCNF2的MP/MC位来重新配置芯片运行模式。
 
说的明白易懂一点,XMP/MC的值影响的是在0x3FFFC0--0x3FFFFF的地址范围上映射的是BROM向量(从ROM中获取)还是XINTF向量(从XINTF Zone7中获取):0为BROM向量,1为XINTF向量;
 
当为微计算机模式,芯片从内部Boot Rom引导;Bootloader通过检测四个通用IO口得状态来确定使用哪种引导模式。四个IO状态及对应的引导模式如下表所示:
 GPIOF4(SCITXDA)  GPIOF12(MDXA)   GPIOF3(SPISTEA)   GPIOF2(***)   引导模式
 PU  No PU   No PU   No PU  GPIO是否内部拉高
 1  X  X  X  Flash引导模式,跳转到Flash地址X3F7FF6
 0  1  X  X  SPI引导模式,调用SPI_Boot,从外部串行SPI EEPROM 启动
 0  0  1  1  SCI引导模式,调用SCI_Boot从SCI-A引导启动
 0  0  1  0  H0 SARAM引导模式,跳转到H0 SARAM地址0x3F8000
 0  0  0  1  OPT引导模式,跳转到OPT地址0x3D7800
 0  0  0  0  并行引导模式,调用Parallel_Boot从通用IO口B口启动
 
最常用的为Flash引导模式,硬件上确保DSP的XMP/MC管脚接地,且SCIATXDA脚不被拉低;
 
当XMP/MC接低电平,表示微计算机模式,那么0x3FFFC0指向的是2812的片内Flash的地址。上电复位后,复位向量是指向片内Flash的0x3FFFC0。2812有一块Boot Rom,地址为0x3FF000--0x3FFFFF,在出厂时已经固化好了引导程序。在0x3FFFC0处是一条跳转指令,跳到iniboot(地址0x3FFB50)函数处执行iniboot代码,该iniboot代码在出厂时已固化在Flash中。iniboot函数判断4个GPIO引脚来判断使用哪一种引导模式,比如Flash boot模式,当SCITXDA为高电平时表明是片内Flash boot模式,那么iniboot执行后跳转到0x3F7FF6处,此位置刚好在128位密码位置之前,你需要自己在0x3F7FF6处放置跳转指令(GEGIN :origin=0x3F7FF6,length=0x000002;codestart :>BEGIN PAGE=0)
 
codestart函数在文件DSP281x_CodeStartBranch.asm中用汇编语言实现的。如下:
 
/**************************************************************/
 
   .sect "codestart"
code_start:
    .if WD_DISABLE == 1
        LB wd_disable      ;Branch to watchdog disable code
    .else
        LB _c_int00        ;Branch to start of boot.asm in RTS library
    .endif
    .if WD_DISABLE == 1
    .text
wd_disable:
    SETC OBJMODE        
    EALLOW              
    MOVZ DP, #7029h>>6  
    MOV @7029h, #0068h  
    EDIS                
    LB _c_int00        
.endif
.end
在0x3F7FF6取出跳转指令,跳转到自己的制定地址或者C初始化的入口_C_INT00处,在C初始化的入口_C_INT00对一些变量,堆栈和寄存器进行必要的设置,该函数在C的库函数内,最后进入Main函数;