This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI提供的库中sgen.calc(&sgen);是什么意思??



在看TI的源码看到sgen.calc(&sgen)。
很疑惑,看不懂。sgen.calc(&sgen);是如何影响gen.out的值?求大神讲解一下运行的过程。
例如:

/* ==============================================================================

System Name:    Complex FFT - Software Test Bench (STB)

File Name:      FFTCD.C

Description:    Primary System file for demonstrating the Complex FFT module

Originator:     Advanced Embeeded Control (AEC) - Texas Instruments

Target dependency:  x28x

Description:
============

*/

#include <stb.h>
#include <fft.h>

/* Create an instance of Signal generator module    */
SGENTI_1 sgen = SGENTI_1_DEFAULTS;

/* Create an instance of DATALOG Module             */
DLOG_4CH dlog=DLOG_4CH_DEFAULTS;      
    
/* Create an Instance of FFT module                 */
#define N   128
#pragma DATA_SECTION(ipcb, "FFTipcb");
#pragma DATA_SECTION(mag, "FFTmag");
CFFT32  fft=CFFT32_128P_DEFAULTS;     
long ipcb[2*N];
long mag[N]; 

/* Define window Co-efficient Array  and place the
.constant section in ROM memory                                */
const long win[N/2]=HAMMING128;

CFFT32_ACQ  acq=CFFT32_ACQ_DEFAULTS;        
    
int xn,yn;
void main()
{    

/* DATALOG module initialisation                    */        
       dlog.iptr1=&xn;
       dlog.iptr2=&yn;
       dlog.trig_value=0x800;
       dlog.size=0x400;         /* Can log 1024 Samples                      */
       dlog.init(&dlog);

/* Signal Generator module initialisation           */ 
       sgen.offset=0;
       sgen.gain=0x7fff;        /* gain=1 in Q15                              */
       sgen.freq=10000;         /* freq = (Required Freq/Max Freq)*2^15       */
                                /*      = (931/3051.7)*2^15 = 10000           */         
       sgen.step_max=10000;     /* Max Freq= (step_max * sampling freq)/65536 */
                                /* Max Freq = (10000*20k)/65536 = 3051.7      */

/* Initialize acquisition module                    */
        acq.buffptr=ipcb;
        acq.tempptr=ipcb;
        acq.size=N;
        acq.count=N;
        acq.acqflag=1;

/* Initialize FFT module                            */
        fft.ipcbptr=ipcb;
        fft.magptr=mag;  
        fft.winptr=(long *)win;
        fft.init(&fft);  

/*---------------------------------------------------------------------------
    Nothing running in the background at present           
----------------------------------------------------------------------------*/

        while(1) 
        {
            sgen.calc(&sgen);
            xn=sgen.out;
            yn=sgen.out;
            dlog.update(&dlog);

            acq.input=((unsigned long)xn)<<16;
            acq.update(&acq);   

            if (acq.acqflag==0)     // If the samples are acquired      
            {   
                CFFT32_brev2(ipcb,ipcb,N);
                CFFT32_brev2(ipcb,ipcb,N);  // Input samples in Real Part
                fft.win(&fft);      
                CFFT32_brev2(ipcb,ipcb,N);
                CFFT32_brev2(ipcb,ipcb,N);  // Input after windowing    
                fft.izero(&fft); 
                fft.calc(&fft);
                fft.mag(&fft); 
                acq.acqflag=1;      // Enable the next acquisition          
            }

        }       

} /* End: main() */