This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单相逆变器TMDSHV1PHINVKIT直流侧电源



我最近在用TMDSHV1PHINVKIT,现在在做并网实验。直流侧380V/2A,交流侧120V/60Hz,按照用户手册步骤进行的。现在有个问题就是一并网合闸,从GUI能看到很短瞬间的normal inverter mode,之后就跳到了DC bus voltage over mode,然后直流电源就下降到0V了,我觉得这里是直流侧电源保护了,但是我不清楚是什么原因导致的。我把直流侧电源的限制电流提高到5A,还是发生上面的问题。我觉得交流侧应该没问题,因为在normal inverter mode,我看到交流电流是2.7A。程序没改,只是设置了INCR_BUILD=3。之前AC侧只接电阻负载是正常工作的。请大家帮忙看看是什么原因,谢谢啦!

  • 你好!不知道你能不能看到这个帖子。我目前也在做TMDSHV1PHINVKIT的调试。也遇到了和你类似的情况。就是在INCR_BUILD=3时,AC侧我直接接的实际电网(220V/50HZ)。DC侧我使用的380V/2A的电源。现在的问题也是用GUI发送后开始可以显示进入normal inverter mode,而且电网电流我通过示波器看到是正弦50HZ的,但是很快就停止工作,显示DC bus voltage over 。不知道是什么问题。想问下你这个问题是否解决了?在E2E上也看到的你关于这个的帖子,但是好像TI给的解释没有太大作用。方便的话加个QQ:1599165211。

  • 不要接实际的电网,接AC交流电源,user guide上写着了

  • 你好!为什么不能接实际的电网? AC交流电源和实际电网应该是一样的吧。还是说程序中有哪些要做修改?

  • 您好!看到您之前用过这个套件,我想请问一下在INCR_BUILD=2的时候,手册上说电流输出为2.71A的有效值,但是我的输出为4A有效值,我实在不知道为什么了,在INCR_BUILD=1时输出了正弦波,INCR_BUILD=2时输出电流却很大,负载为44欧姆电阻,功率也很大。希望能够得到您的帮助,谢谢!